EAGLE User Support (English) Cannot place any component in the board in the freeware licensed eagle cad
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 379 views
  • Users 0 members are here
  • board
  • eagle
  • question
Related

Cannot place any component in the board in the freeware licensed eagle cad

Former Member
Former Member over 13 years ago

Hello,

         I have a freeware version of eagle cad 6.3.0.

        

I'm trying to build a custom board for my project using only 3 surface mount ic's. i have build a library file for the IC I require of a size 8.83x7mm. when i try to place it on my board design it shows an error

 

"the lite edition of eagle cannot perform this action. Some objects extend outside the board area"

 

It shows me this error even when i try to place any component from the pre-installed library.

 

The attached file shows the error message

 

Please help me with this..

Attachments:
image
  • Sign in to reply
  • Cancel
  • fritzz
    0 fritzz over 13 years ago

    You only get to use a small area in the upper right quadrant above that + you see on the screem. Make sure your board is there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago in reply to fritzz

    Thank you so much. It was very helpful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fritzz
    0 fritzz over 13 years ago in reply to Former Member

    Happy to help. I was new to Eagle not that long ago.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to fritzz

    Okay - that's all good and well, but how do I define the board area if it is a different shape than a square board, a circle for example, or some other random shape, for esthetic purposes?