Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to chamfer a PCB edge connector
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 3256 views
  • Users 0 members are here
Related

How to chamfer a PCB edge connector

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

I am wrestling with a problem creating a new library device. It is an edge connector, and the manufacturer recommends a 45 degree chamfer on the PCB edge see http://www.samtec.com/documents/webfiles/cpdf/MEC2-XX-XX-X-D-DV-X-FOOTPRINT.pdf

 

Presumably this is to help the PCB guide properly into the connector and I am not sure how to do this, I am a relative newbie to EAGLE but not CAD software. Creating new parts was no problem till I hit this.

 

Could someone share their secret?

 

thanks in advance

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    On Fri, 18 Jan 2013 12:46:56 GMT, Paul Anderson

    <noreply-144097@element14.com> wrote:

     

    >Thanks, and yes I should have noted the chamfer in question was on Sheet 3 to avoid the guesswork in answering my question, Drawing View 22 where it says "0.30 x 45 (BOTH SIDES)". This is a third dimension feature to bevel off the PCB edge and as far as I could tell EAGLE libraries work in 2 dimensions. I'll make a note to the fab house when I submit the Gerbers, and also note the gold finish is on the tFinish/bFinish layers (I started by copying package PCI-SLOT-60 from the standard con-amp.lbr and modifying it).

     

     

    Typicall you would give the board house a Drill Drawing, that outlines

    the drills and their placement, along with any other details like

    Dimensions, board stackup/material, UL marking, masking, screening

    color, finish(HASL etc), milling, stackup registration, warp/twist

    tolerances and chamfers etc.  The edge connector detail is outlined in

    this drawing, including gold finishing.  It allows a fast quote since

    all the details for the board ( dimensions stackup etc) are on the

    Drill Drawing.

     

     

     

    Cheers

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks, and yes I should have noted the chamfer in question was on Sheet 3 to avoid the guesswork in answering my question, Drawing View 22 where it says "0.30 [.012] x 45 (BOTH SIDES)". This is a third dimension feature to bevel off the PCB edge and as far as I could tell EAGLE libraries work in 2 dimensions. I'll make a note to the fab house when I submit the Gerbers, and also note the gold finish is on the tFinish/bFinish layers (I started by copying package PCI-SLOT-60 from the standard con-amp.lbr and modifying it).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Paul Anderson wrote:

     

    Hello,

     

    I am wrestling with a problem creating a new library device. It is an edge

    connector, and the manufacturer recommends a 45 degree chamfer on the PCB

    edge see

    http://www.samtec.com/documents/webfiles/cpdf/MEC2-XX-XX-X-D-DV-X-

    FOOTPRINT.pdf

     

    Presumably this is to help the PCB guide properly into the connector and I

    am not sure how to do this, I am a relative newbie to EAGLE but not CAD

    software. Creating new parts was no problem till I hit this.

     

    Could someone share their secret?

     

    thanks in advance

     

    No secret. Eagle isn't a mechanical design package. Anything that involves

    more than plunging a router or drill bit through a thickness of PCB material

    involves making fab notes on the fabrication print and communicating the

    necessary work to the board house. Even board thickness needs to be

    communicated in that fashion.

     

    For that connector, I'd lay out the package footprint as Samtec describes,

    and then make a note in the symbol description stating how far back the

    origin of the symbol should be from the edge of the board. When I placed

    that symbol I would then know how far back from the board edge to place it

    to account for the chamfer (Samtec has already done the math for you to

    provide the proper pad clearance).

     

    I would then make a copy of the chamfer drawing Samtec provides somewhere on

    the fabrication print, using lines, arcs, whatever, and referencing the

    appropriate edge of the PCB. I'd add a fab note to that effect as well.

    Finally, I would communicate with the board house that a chamfer was

    required when I submitted the board for production. At pretty much every

    board house I use a chamfer is a 'full-featured' custom PCB quote (along

    with the necessary gold plating, which is another fab note.)

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi Paul,

     

    I cannot open your link, but I think what you indicated is the "Gold

    finger" chamfer? If right and you need to insert this board to a device. We

    also suggest 45 degree for better connection.

     

    In our company, we also will suggest our clients to do the chamfer if the

    board will be used as connection.

     

    Regards,

    Lynn

    mailto:sales@real-pcb.com

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.