Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How to delete device(s) from an eagle library ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 2647 views
  • Users 0 members are here
Related

How to delete device(s) from an eagle library ?

manes6969
manes6969 over 13 years ago

Does anybody know how to do this ? Just can not find it ...

Greetings Ronny

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 11.02.2013 14:31, ronny suy wrote:

    Does anybody know how to do this ? Just can not find it ...

    Greetings Ronny

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/69387#69387/l/how-to-delete-devices-from-an-eagle-library

     

     

     

    This can be done in the Library/Remove.... menu or with the REMOVE

    command.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 11.02.2013 14:31, ronny suy wrote:

    Does anybody know how to do this ? Just can not find it ...

    Greetings Ronny

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/69387#69387/l/how-to-delete-devices-from-an-eagle-library

     

     

     

    This can be done in the Library/Remove.... menu or with the REMOVE

    command.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I have very similar question to original post.  Library/Remove or REMOVE command works, but it is very inefficient.  Is there a way to clear several items at once?

     

    Here is the usage challenge:  When creating a new library, and with a desire to import existing packages for parts into that new library, it seems like making a copy of an existing library (which contains many nice clean common packages), then renaming and deleting all the devices and symbols, but leaving the packages would be a simple path.  However, I can not see any efficient way to delete devices or symbols.

     

    Actually, just to generally comment, as much as I like using Eagle (currently using v6.6), the library management is a bit painful.  It feels like a neglected portion of the platform, although it is probably easier than other platforms.  It would be nice to have the option to globally manage packages and/or link them across multiple libraries.  For example:  I might have tweeked the SOIC-14N package in my Texas.lbr, and I want to have all chip libraries start using the same SOIC-14N package.  Currently, the only method for doing this, that I know of, is to individually copy and paste all the existing layered bits of the packages into the other libraries.  Of course this does work... but it is terribly inefficient.  Perhaps I need to suggest a new library class, or "special" library, perhaps global_packages.lbr that has only packages, and then add the ability for other libraries' devices to link to those global_packages.lbr packages, while not changing the current ability for each library to have its own set of packages and symbols.  Therefore any linked global packages would show up as a separate "variant" not replacing existing packages.

     

    Thank you.