EAGLE User Support (English) Script file drill size
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
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 276 views
  • Users 0 members are here
Related

Script file drill size

autodeskguest
autodeskguest over 17 years ago

Hello,

I have recently started using Eagle (ver. 5.1.0) and am trying to create a

script file to generate my board (it is easiest for me to make the script

file for what I am doing).  I would like to place vias with hole size of

0.01" and diameter 0.015".  I put in the command:

 

CHANGE DRILL diameter 0.01;

and then:

Via 0.01 ROUND 1-2 (0.10 0.16);

 

When I run the script I get an error:

"Invalid pad drill: "Diameter 0.01"

(valid range is 0.000004..0.516024inch)

 

and Eagle puts a via in the right place with diameter 0.01 and drill

0.023622

Any suggestions as to what I am doing wrong

thank you in advance

David

 

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    David Stevens wrote:

    Hello,

    I have recently started using Eagle (ver. 5.1.0) and am trying to create a

    script file to generate my board (it is easiest for me to make the script

    file for what I am doing).  I would like to place vias with hole size of

    0.01" and diameter 0.015".  I put in the command:

     

    CHANGE DRILL diameter 0.01;

    and then:

    Via 0.01 ROUND 1-2 (0.10 0.16);

     

    When I run the script I get an error:

    "Invalid pad drill: "Diameter 0.01"

    (valid range is 0.000004..0.516024inch)

     

    and Eagle puts a via in the right place with diameter 0.01 and drill

    0.023622

     

    Are you sure about this - the drill cannot be less than the pad- the actual

    pad diameter gets changed by Eagle in this case

     

    Any suggestions as to what I am doing wrong

    thank you in advance

    David

     

     

     

     

    In any case the first line should just be:

     

    change drill 0.01;   you do not need diameter in there

     

      You also leave an annular ring of only 0.0025" - there is hardly any

    copper there! Eagles DRC check parameters will need to be changed to

    accommodate all of this or else Eagle will automatically increase the

    annular ring- see the restring parameters.

     

    The second parameter in the via line should be the pad diameter, I take it

    this is just a typo

     

    cheers

     

    David