Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 6 : Problem Importing Custom Parts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1317 views
  • Users 0 members are here
  • eagle_v6
  • pcb_design
  • pcb_socket
  • eagle_library
Related

Eagle 6 : Problem Importing Custom Parts

e14 Contributor
e14 Contributor over 13 years ago

Recently started working on a new PCB board for a dev kit. I ran in an issue where I had made a custom part for the M50-3501042M50-3501042 2x10 male header with 0.05'' (1.27mm) pitch.

Note also that this is a through-hole component.

The issue I had was that I set the diameter of each of the pins in the custom package to 0.04'', however, when I imported the part into my PCB design, the pins on the board had increased in diameter and were overlapping with other pins giving DRC errors.

I updated the library and all the parts in Eagle, however, this did not fix my issue.

I have no idea on how to fix this issue. Any ideas?

Originally posted: http://electronics.stackexchange.com/questions/59580/eagle-6-problem-importing-custom-parts

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 03/02/2013 08:24 PM, Edwin Chand wrote:

    Recently started working on a new PCB board for a dev kit. I ran in an issue where I had made a custom part for the M50-3501042M50-3501042 2x10 male header with 0.05'' (1.27mm) pitch.

    Note also that this is a through-hole component.

    The issue I had was that I set the diameter of each of the pins in the custom package to 0.04'', however, when I imported the part into my PCB design, the pins on the board had increased in diameter and were overlapping with other pins giving DRC errors.

    I updated the library and all the parts in Eagle, however, this did not fix my issue.

    I have no idea on how to fix this issue. Any ideas?

    Originally posted: http://electronics.stackexchange.com/questions/59580/eagle-6-problem-importing-custom-parts

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/71141#71141/l/eagle-6-problem-importing-custom-parts

     

    The data sheet recommends 0.70+-05 mm or 27.5 mil for the drill.

    The DRC sets the restring size.

    It will be a tight fit.

    Paul R.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I reduced the Rest Ring pad min spacings to 6 mil instead and got the DRC to pass w/o overlaps. Setting the percentage to 0% for the rest ring as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I reduced the Rest Ring pad min spacings to 6 mil instead and got the DRC to pass w/o overlaps. Setting the percentage to 0% for the rest ring as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer