EAGLE User Support (English) Is it possible to REALLY disable the alpha-blending WITH a white background?
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
  • Replies 7 replies
  • Subscribers 178 subscribers
  • Views 678 views
  • Users 0 members are here
Related

Is it possible to REALLY disable the alpha-blending WITH a white background?

autodeskguest
autodeskguest over 17 years ago

According to the UPDATE_en text file

 

- If you want to have the old raster OP behavior on black background,

    you can uncheck the "Use alpha blending" box in the "Options/Set/Colors"

    dialog. In that case the alpha value defined for the colors is ignored

    when using a black background, and colors are mixed using an OR

    function.

 

Why only a black background? Why did it work with a white background before.

I have a colour deficiency (like a lot of the male population) and red does

not stand out well from black in the schematic. Switching from one white

screen to a black one is really good for eyestrain. I work on both the sch

and the pcb.

 

What on earth is the point of the alpha-blending in the schematic in any

case. Why would you want to superimpose objects?

 

--

Martin Hodges

Senior design engineer

Network Electronics ASA

 

 

  • Sign in to reply
  • Cancel
Parents
  • kcadsoft
    kcadsoft over 17 years ago

    On 10/16/08 13:40, Martin Hodges wrote:

    According to the UPDATE_en text file

     

    - If you want to have the old raster OP behavior on black background,

        you can uncheck the "Use alpha blending" box in the "Options/Set/Colors"

        dialog. In that case the alpha value defined for the colors is ignored

        when using a black background, and colors are mixed using an OR

        function.

     

    Why only a black background? Why did it work with a white background before.

     

    Mixing colors with raster OPs only works really useful with an OR operation,

    which implies a black background. On a white background only an "AND-NOT"

    operation can be done, and even that leads to all-black pretty soon.

     

    I have a colour deficiency (like a lot of the male population) and red does

    not stand out well from black in the schematic. Switching from one white

    screen to a black one is really good for eyestrain. I work on both the sch

    and the pcb.

     

    What on earth is the point of the alpha-blending in the schematic in any

    case. Why would you want to superimpose objects?

     

    All graphics editors in EAGLE use the same drawing engine.

     

    If you don't want to have alpha blending on a white background, you can

    set the alpha value of all colors to 255, which will make them fully opaque.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Hofmark 2                               Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kcadsoft
    kcadsoft over 17 years ago

    On 10/16/08 13:40, Martin Hodges wrote:

    According to the UPDATE_en text file

     

    - If you want to have the old raster OP behavior on black background,

        you can uncheck the "Use alpha blending" box in the "Options/Set/Colors"

        dialog. In that case the alpha value defined for the colors is ignored

        when using a black background, and colors are mixed using an OR

        function.

     

    Why only a black background? Why did it work with a white background before.

     

    Mixing colors with raster OPs only works really useful with an OR operation,

    which implies a black background. On a white background only an "AND-NOT"

    operation can be done, and even that leads to all-black pretty soon.

     

    I have a colour deficiency (like a lot of the male population) and red does

    not stand out well from black in the schematic. Switching from one white

    screen to a black one is really good for eyestrain. I work on both the sch

    and the pcb.

     

    What on earth is the point of the alpha-blending in the schematic in any

    case. Why would you want to superimpose objects?

     

    All graphics editors in EAGLE use the same drawing engine.

     

    If you don't want to have alpha blending on a white background, you can

    set the alpha value of all colors to 255, which will make them fully opaque.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Hofmark 2                               Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 17 years ago in reply to kcadsoft

    Klaus Schmidinger wrote:

     

    On 10/16/08 13:40, Martin Hodges wrote:

    According to the UPDATE_en text file

     

    - If you want to have the old raster OP behavior on black background,

        you can uncheck the "Use alpha blending" box in the

        "Options/Set/Colors" dialog. In that case the alpha value defined for

        the colors is ignored when using a black background, and colors are

        mixed using an OR function.

     

    Why only a black background? Why did it work with a white background

    before.

     

    Mixing colors with raster OPs only works really useful with an OR

    operation, which implies a black background. On a white background only an

    "AND-NOT" operation can be done, and even that leads to all-black pretty

    soon.

     

    I have a colour deficiency (like a lot of the male population) and red

    does not stand out well from black in the schematic. Switching from one

    white screen to a black one is really good for eyestrain. I work on both

    the sch and the pcb.

     

    What on earth is the point of the alpha-blending in the schematic in any

    case. Why would you want to superimpose objects?

     

    All graphics editors in EAGLE use the same drawing engine.

     

    If you don't want to have alpha blending on a white background, you can

    set the alpha value of all colors to 255, which will make them fully

    opaque.

     

    Klaus Schmidinger

     

    Thank you for the tip about the palette. It is not very intuitive though.

    The different background buttons are not obviously buttons on linux.

     

    One cpu killer for me was the use of a large cursor. Switch to the small

    cursor for a hardware accelerated cursor!! Moving the cursor around the

    screen used up 50% cpu. I do not know why the performace difference is so

    large between v4 and v5 with the large cursor though.

     

    The drawing engine is horribly slow compared to v4. I dread having to use v5

    for a project.

     

    I REALLY regret having saved a project in v5. Going back to v4 is no longer

    possible.

     

    --

    Martin Hodges

    Senior design engineer

    Network Electronics ASA

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 17 years ago in reply to autodeskguest

    On 10/16/08 18:33, Martin Hodges wrote:

    ...

    The different background buttons are not obviously buttons on linux.

     

    Which buttons are you referring to?

    Can you provide a screenshot?

     

    One cpu killer for me was the use of a large cursor. Switch to the small

    cursor for a hardware accelerated cursor!! Moving the cursor around the

    screen used up 50% cpu. I do not know why the performace difference is so

    large between v4 and v5 with the large cursor though.

     

    In version 4 we could draw the large cursor with the XOR raster OP, directly

    to the widget on screen. Version 5 is based on Qt 4, which, unfortunately,

    had totally abandoned raster OP capabilities. Therefore we now need to

    redraw large parts of the screen widget when drawing the large cursor.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Hofmark 2                               Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________