EAGLE User Support (English) Is it possible to REALLY disable the alpha-blending WITH a white background?
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
  • Replies 7 replies
  • Subscribers 178 subscribers
  • Views 678 views
  • Users 0 members are here
Related

Is it possible to REALLY disable the alpha-blending WITH a white background?

autodeskguest
autodeskguest over 17 years ago

According to the UPDATE_en text file

 

- If you want to have the old raster OP behavior on black background,

    you can uncheck the "Use alpha blending" box in the "Options/Set/Colors"

    dialog. In that case the alpha value defined for the colors is ignored

    when using a black background, and colors are mixed using an OR

    function.

 

Why only a black background? Why did it work with a white background before.

I have a colour deficiency (like a lot of the male population) and red does

not stand out well from black in the schematic. Switching from one white

screen to a black one is really good for eyestrain. I work on both the sch

and the pcb.

 

What on earth is the point of the alpha-blending in the schematic in any

case. Why would you want to superimpose objects?

 

--

Martin Hodges

Senior design engineer

Network Electronics ASA

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Martin Hodges wrote:

    Klaus Schmidinger wrote:

     

    On 10/16/08 13:40, Martin Hodges wrote:

    According to the UPDATE_en text file

     

    - If you want to have the old raster OP behavior on black

        background, you can uncheck the "Use alpha blending" box in the

        "Options/Set/Colors" dialog. In that case the alpha value

        defined for the colors is ignored when using a black

        background, and colors are mixed using an OR function.

     

    Why only a black background? Why did it work with a white background

    before.

     

    Mixing colors with raster OPs only works really useful with an OR

    operation, which implies a black background. On a white background

    only an "AND-NOT" operation can be done, and even that leads to

    all-black pretty soon.

     

    I have a colour deficiency (like a lot of the male population) and

    red does not stand out well from black in the schematic. Switching

    from one white screen to a black one is really good for eyestrain.

    I work on both the sch and the pcb.

     

    What on earth is the point of the alpha-blending in the schematic

    in any case. Why would you want to superimpose objects?

     

    All graphics editors in EAGLE use the same drawing engine.

     

    If you don't want to have alpha blending on a white background, you

    can set the alpha value of all colors to 255, which will make them

    fully opaque.

     

    Klaus Schmidinger

     

    Thank you for the tip about the palette. It is not very intuitive

    though. The different background buttons are not obviously buttons on

    linux.

     

    One cpu killer for me was the use of a large cursor. Switch to the

    small cursor for a hardware accelerated cursor!! Moving the cursor

    around the screen used up 50% cpu. I do not know why the performace

    difference is so large between v4 and v5 with the large cursor though.

     

    The drawing engine is horribly slow compared to v4. I dread having to

    use v5 for a project.

     

    I REALLY regret having saved a project in v5. Going back to v4 is no

    longer possible.

     

    Martin, to get your project back to v4 -

    From Cadsoft website, you can find export-schematic.ulp and

    export-board.ulp. Download these and run them on your v5 project to create

    script files that you can then use to rebuild your project in v4. You'll

    probably find there is some tidying up to do - I had some trouble with

    details like text fonts, via drill sizes etc, but it saved a lot of work!

     

    HTH

    --

    Colin

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Martin Hodges wrote:

    Klaus Schmidinger wrote:

     

    On 10/16/08 13:40, Martin Hodges wrote:

    According to the UPDATE_en text file

     

    - If you want to have the old raster OP behavior on black

        background, you can uncheck the "Use alpha blending" box in the

        "Options/Set/Colors" dialog. In that case the alpha value

        defined for the colors is ignored when using a black

        background, and colors are mixed using an OR function.

     

    Why only a black background? Why did it work with a white background

    before.

     

    Mixing colors with raster OPs only works really useful with an OR

    operation, which implies a black background. On a white background

    only an "AND-NOT" operation can be done, and even that leads to

    all-black pretty soon.

     

    I have a colour deficiency (like a lot of the male population) and

    red does not stand out well from black in the schematic. Switching

    from one white screen to a black one is really good for eyestrain.

    I work on both the sch and the pcb.

     

    What on earth is the point of the alpha-blending in the schematic

    in any case. Why would you want to superimpose objects?

     

    All graphics editors in EAGLE use the same drawing engine.

     

    If you don't want to have alpha blending on a white background, you

    can set the alpha value of all colors to 255, which will make them

    fully opaque.

     

    Klaus Schmidinger

     

    Thank you for the tip about the palette. It is not very intuitive

    though. The different background buttons are not obviously buttons on

    linux.

     

    One cpu killer for me was the use of a large cursor. Switch to the

    small cursor for a hardware accelerated cursor!! Moving the cursor

    around the screen used up 50% cpu. I do not know why the performace

    difference is so large between v4 and v5 with the large cursor though.

     

    The drawing engine is horribly slow compared to v4. I dread having to

    use v5 for a project.

     

    I REALLY regret having saved a project in v5. Going back to v4 is no

    longer possible.

     

    Martin, to get your project back to v4 -

    From Cadsoft website, you can find export-schematic.ulp and

    export-board.ulp. Download these and run them on your v5 project to create

    script files that you can then use to rebuild your project in v4. You'll

    probably find there is some tidying up to do - I had some trouble with

    details like text fonts, via drill sizes etc, but it saved a lot of work!

     

    HTH

    --

    Colin