EAGLE User Support (English) Is it possible to REALLY disable the alpha-blending WITH a white background?
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
  • Replies 7 replies
  • Subscribers 178 subscribers
  • Views 680 views
  • Users 0 members are here
Related

Is it possible to REALLY disable the alpha-blending WITH a white background?

autodeskguest
autodeskguest over 17 years ago

According to the UPDATE_en text file

 

- If you want to have the old raster OP behavior on black background,

    you can uncheck the "Use alpha blending" box in the "Options/Set/Colors"

    dialog. In that case the alpha value defined for the colors is ignored

    when using a black background, and colors are mixed using an OR

    function.

 

Why only a black background? Why did it work with a white background before.

I have a colour deficiency (like a lot of the male population) and red does

not stand out well from black in the schematic. Switching from one white

screen to a black one is really good for eyestrain. I work on both the sch

and the pcb.

 

What on earth is the point of the alpha-blending in the schematic in any

case. Why would you want to superimpose objects?

 

--

Martin Hodges

Senior design engineer

Network Electronics ASA

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Klaus Schmidinger wrote:

     

    On 10/16/08 18:33, Martin Hodges wrote:

    ...

    The different background buttons are not obviously buttons on linux.

     

    Which buttons are you referring to?

    Can you provide a screenshot?

     

     

    Attached.

     

    One cpu killer for me was the use of a large cursor. Switch to the small

    cursor for a hardware accelerated cursor!! Moving the cursor around the

    screen used up 50% cpu. I do not know why the performace difference is so

    large between v4 and v5 with the large cursor though.

     

    In version 4 we could draw the large cursor with the XOR raster OP,

    directly to the widget on screen. Version 5 is based on Qt 4, which,

    unfortunately, had totally abandoned raster OP capabilities. Therefore we

    now need to redraw large parts of the screen widget when drawing the large

    cursor.

     

    Klaus Schmidinger

     

    That explains a lot.

    The world does strange things in the name of progress...

     

    Again, thanks for the follow-up.

     

    M

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Klaus Schmidinger wrote:

     

    On 10/16/08 18:33, Martin Hodges wrote:

    ...

    The different background buttons are not obviously buttons on linux.

     

    Which buttons are you referring to?

    Can you provide a screenshot?

     

     

    Attached.

     

    One cpu killer for me was the use of a large cursor. Switch to the small

    cursor for a hardware accelerated cursor!! Moving the cursor around the

    screen used up 50% cpu. I do not know why the performace difference is so

    large between v4 and v5 with the large cursor though.

     

    In version 4 we could draw the large cursor with the XOR raster OP,

    directly to the widget on screen. Version 5 is based on Qt 4, which,

    unfortunately, had totally abandoned raster OP capabilities. Therefore we

    now need to redraw large parts of the screen widget when drawing the large

    cursor.

     

    Klaus Schmidinger

     

    That explains a lot.

    The world does strange things in the name of progress...

     

    Again, thanks for the follow-up.

     

    M

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kcadsoft
    kcadsoft over 17 years ago in reply to autodeskguest

    On 10/19/08 23:38, Martin Hodges wrote:

    Klaus Schmidinger wrote:

     

    On 10/16/08 18:33, Martin Hodges wrote:

    ...

    The different background buttons are not obviously buttons on linux.

    Which buttons are you referring to?

    Can you provide a screenshot?

     

     

    Attached.

     

    Well, they look like buttons to me.

     

    How do you suggest they should look?

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Hofmark 2                               Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________