Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Push button leg functions?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1392 views
  • Users 0 members are here
  • push
  • plunger
  • button
Related

Push button leg functions?

e14 Contributor
e14 Contributor over 13 years ago

With a plugner button like this that has 3 legs. What would dose each function do? as normally my buttons just have two legs and it dosent matter which order I connect them up aslong as both are connected.

 

http://www.digikey.com/product-search/en?mpart=982A01RX&vendor=137

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 13 years ago

    Hi Matt,

    This pdf shows that model 982A01RX982A01RX follows the pinout designated 1A,

    which in the table in the PDF shows that pins 2 and 3 are the ones you should use.

    The manufacturer also makes different variations and in that case the additional pins get used.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Thanks alot Shabaz your really helpfull!

     

    Please could you take a look at this one

     

    http://www.e-switch.com/Portals/0/Series_Pdf/5500.pdf

     

     

    Im using 5511 (2nd page, 2nd from top. wide black button with one green led)

     

    I understand the led legs of course, but once again there is then 4 legs for the button Im not quiet sure which ones I should trace with my pcb.

     

    Thanks again Shabaz!

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Thanks alot Shabaz your really helpfull!

     

    Please could you take a look at this one

     

    http://www.e-switch.com/Portals/0/Series_Pdf/5500.pdf

     

     

    Im using 5511 (2nd page, 2nd from top. wide black button with one green led)

     

    I understand the led legs of course, but once again there is then 4 legs for the button Im not quiet sure which ones I should trace with my pcb.

     

    Thanks again Shabaz!

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to e14 Contributor

    Am 08.05.2013 21:07, schrieb Matt Porta:

    Thanks alot Shabaz your really helpfull!

     

    Please could you take a look at this one

     

    http://www.e-switch.com/Portals/0/Series_Pdf/5500.pdf

     

     

    Im using 5511 (2nd page, 2nd from top. wide black button with one green

    led)

     

    I understand the led legs of course, but once again there is then 4 legs

    for the button Im not quiet sure which ones I should trace with my pcb.

     

    Thanks again Shabaz!

     

    Matt

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/76045#76045

     

     

    Look at the 5511 3-sides view. The bottom view shows the pins with

    numbers 1-3 and 1-2.

    Look at the schematic picture of the switch and you can see that the

    common (1) is connected to 2 pins, N.O. pin to (3) and N.C. pin to (2).

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    Hi Matt,

     

    Basically the NC and NO indicate normally-closed and normally-open, so one of the other two pins has to be the 'common' pin. In the case of this particular switch

    (actually many switches) more than one pin can be used for the same function. So, the two pins marked '1' are the 'common' pin.

    If you want a switch that connects when you press it, then you can use the NO pin, and either of the two pins marked '1'; just select the one that is convenient for your layout.