EAGLE User Support (English) eagle ignores command line options
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 598 views
  • Users 0 members are here
Related

eagle ignores command line options

Former Member
Former Member over 12 years ago

Eagle 6.2 & 6.4

 

On both linux and windows in both 6.2 and 6.4 I can't get the ealge command line options to have any affect.  For example, the trivial "eagle -Cquit" opens eagle and leaves it open.  More to my needs, "eagle -Stest.scr" does not execute test.scr.  I don't get any error messages or any indication that eagle even saw the command line option.  However, if i try "eagle -C" i do get an error: "Missing parameter for option -S"

 

Can anyone shed some insight into what would cause this kind of behavior, or how to get eagle to execute the script from the command line options?

 

Thanks!!

  • Sign in to reply
  • Cancel
  • dukepro
    0 dukepro over 12 years ago

    George,

     

    I observed the same behavior when a drawing or project file was not also

    specified.  Try this:

     

        cd /path/to/project

        eagle -C quit eagle.epf

     

    It works as described.

     

    Here's an excerpt from the 6.4 user manual, Section 10.3 "EAGLE Options

    at a Glance" on page 306 of the English version:

     

        -C

        Execute a command

        After loading an EAGLE file the given command will be

        executed in the Editor window's command line.

        See also help function, Command Line Options.

     

    HTH,

        - Chuck

     

     

    On 05/14/2013 12:19 AM, George Nunya wrote:

    Eagle 6.2 & 6.4

     

    On both linux and windows in both 6.2 and 6.4 I can't get the ealge

    command line options to have any affect.  For example, the trivial

    "eagle -Cquit" opens eagle and leaves it open.  More to my needs, "eagle

    -Stest.scr" does not execute test.scr.  I don't get any error messages

    or any indication that eagle even saw the command line option.  However,

    if i try "eagle -C" i do get an error: "Missing parameter for option -S"

     

    Can anyone shed some insight into what would cause this kind of

    behavior, or how to get eagle to execute the script from the command

    line options?

     

    Thanks!!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/76626#76626

     

     

     

     

    Attachments:
    7827.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago

    Thanks Chuck

     

    That was exactly the problem!  Pretty subtle detail there, thank you very much for pointing it out.

     

    George