Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) ULP: Create reliable temp filename for scripts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 191 subscribers
  • Views 3037 views
  • Users 0 members are here
  • ulp
  • mac
Related

ULP: Create reliable temp filename for scripts

e14 Contributor
e14 Contributor over 13 years ago

Hello,

as far as I understand, the only way to manipulate the data structure of either an eagle schematic, board or library through an ULP is to collect the necessary commands in a text file and execute it using exit ("script <filename>"). This method works as long as there is a suitable filename available that is writeable. On a unix system, this would be somewhere in /tmp, on windows, this would be some other location. I have failed so far to find a way to create a temporary filename that works across all supported operating systems. I suggest to add a function to create a temporary path for exactly that purpose and to document it together with the whole approach of collecting commands to manipulate the data structure in a script and execute that script after the ULP is finished. This would have the other advantage that the script could get deleted after execution because it is intended for a single execution anyway.

 

What do you think about this? Does anyone has a realiable solution to create a temporary filename? I think the currently most used approach is to place the script into the same directory as the currently edited schematic or library. This works because the user usually has the rights to write to the directory of the currently edited file. But I think this is a hack because the file remains after execution and does not belong there. Another interesting idea would be to have a magic filename, for example ":memory" so the commands get stored somewhere in memory, exeuted and never become an object in the users filesystem.

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to CSWalt

    Walter Spermann wrote on Thu, 27 June 2013 05:40

    Hi,

     

    ]

    if you have a loop that does a concatenation in each step like

    "

    string Result;

    string Lines[]; // say 100000 lines filled with some strings

    for (int i=0; i<100000; ++i)

       Result += Lines[i];

    "

    then in each step a reallocation occurs for Result which takes time.

    In that case strjoin is much better:

    "

    Result = strjoin(Lines,'');

    "

    strjoin does the whole thing in one step, only one reallocation and

    copy.

    Hope this makes it clearer.

     

     

    Thanks for the information Walter.

     

    To all.

    I have had a further play. I wondered how the final string size affected

    performance. I found once the size exceeded 132KB the times increased

    dramatically. The graph headed for the heavens.

    That size string would not be common so is probably not relevant

     

    sprintf() has a far more dramatic effect. The attached ULP illustrates

    this.

    So, in some ULPs it would be worth using sprintf() sparingly.

     

    I noticed when running the ULP that the reported times varied quite a bit

    with either of the top two sprintf techniques  being the faster. The string

    size remained the same so I can only imagine there is contention for

    resources when this is observed. 

     

    Regards

    Warren

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    Avoidsprintf.ulp.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • CSWalt
    0 CSWalt over 13 years ago in reply to autodeskguest

    Hi,

     

    On 06/25/13 20:04, Jorge Garcia wrote:

    On 6/25/2013 8:56 AM, Chuck Huber wrote:

    On 06/25/2013 05:13 AM, KimP wrote:

     

    Good finding(s), never thought there would be such a huge difference

    between string handling (variable vs array). Although, in real-world

    ULPs I don't think these details make such a big difference, they

    might reveal some areas for improvement.

     

    Jorge,  Would it be possible to ask one of the developers to provide

    some enlightenment on how strings and string arrays are handled?

     

    Thanks,

         - Chuck

     

    Hi Chuck,

     

    I'll see what I can do. I've tried the ULP on my linux box and the

    strjoin operation was always faster than the concatenation. However both

    were at least an order of magnitude slower than writing the script file.

     

    I'm sure they'll be very interested in this experiment you guys have

    carried out.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

    if you have a loop that does a concatenation in each step like

    "

    string Result;

    string Lines[]; // say 100000 lines filled with some strings

    for (int i=0; i<100000; ++i)

       Result += Lines[i];

    "

    then in each step a reallocation occurs for Result which takes time.

    In that case strjoin is much better:

    "

    Result = strjoin(Lines,'');

    "

    strjoin does the whole thing in one step, only one reallocation and copy.

    Hope this makes it clearer.

     

    Regards,

    Walter Spermann

     

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to dukepro

    On 6/25/2013 8:56 AM, Chuck Huber wrote:

    On 06/25/2013 05:13 AM, KimP wrote:

     

    Good finding(s), never thought there would be such a huge difference

    between string handling (variable vs array). Although, in real-world

    ULPs I don't think these details make such a big difference, they

    might reveal some areas for improvement.

     

    Jorge,  Would it be possible to ask one of the developers to provide

    some enlightenment on how strings and string arrays are handled?

     

    Thanks,

         - Chuck

     

    Hi Chuck,

     

    I'll see what I can do. I've tried the ULP on my linux box and the

    strjoin operation was always faster than the concatenation. However both

    were at least an order of magnitude slower than writing the script file.

     

    I'm sure they'll be very interested in this experiment you guys have

    carried out.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 13 years ago in reply to k.portman

    On 06/25/2013 05:13 AM, KimP wrote:

     

    Good finding(s), never thought there would be such a huge difference

    between string handling (variable vs array). Although, in real-world

    ULPs I don't think these details make such a big difference, they

    might reveal some areas for improvement.

     

    Jorge,  Would it be possible to ask one of the developers to provide

    some enlightenment on how strings and string arrays are handled?

     

    Thanks,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • k.portman
    0 k.portman over 13 years ago in reply to autodeskguest

    The answer is the difference in time it takes Eagle to fetch a string

    compared to an array element.

     

    string a[] = {"test"};

    string b = "test";

     

    runtext += b;

    runtext += a[0];

     

    These run at very different speeds.

     

    Good finding(s), never thought there would be such a huge difference

    between string handling (variable vs array). Although, in real-world

    ULPs I don't think these details make such a big difference, they might

    reveal some areas for improvement.

     

    In coding ULPs I believe more performance is gained by good and simple

    code+data structures. I have not run into situations where ULPs run for

    endless seconds/minutes, but can imagine some possible cases (example

    netlist/footprint conversions) where the ULP execution time builds up

    and becomes critical.

     

    Kim

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to k.portman

    KimP wrote:

    Il 24/06/2013 02:30, Warren Brayshaw ha scritto:

    I timed it again using a Win7 32bit Dual Core mailto:T6670@2.20GHz

     

    On the first pass the strJoin was 82% of the Concatenation time

     

    Subsequent passes averaged 65% of the Concatenation time and quite

    consistant.

     

    So although strJoin took longer on the first pass it was always

    faster than concatenation.

     

    Hi Warren,

     

    First, thanks for writing the test ULP to time the 2 solutions!

    I can confirm your results, the first run gives 91% and second 73%

    speed between strjoin vs concatenation. With 100.000 loops I get

    times on the order of 60 to 70ms, running on Core2-Duo 3.16GHz

    Win-7/64bit.

     

    Now, I suggest to broaden the test cases a little bit, here's why:

    Often there is a need to build more complex commands, using sprintf.

    On some system ULPs I can see code like this:

    =============

    string Cmd, h;

    sprintf(h, "EDIT %s.PaC;\nGRID %s;\n", s[0], Unit);

    Cmd += h;

    =============

     

    In this kind of cases sprintf() formatting becomes beneficial, else

    you have to write something like following (hardly readable):

    =============

    Cmd = "EDIT "s[0]".PaC;\nGRID "Unit+";\n";

    =============

     

    If I modify your test ULP inside the loops like this:

    =============

    for(i=1; i<100000; i++){

    string s;

    sprintf(s, " %s", words[i & 3]);

    runtext += s;

    }

     

    for(i=1; i<100000; i++){

    sprintf(a[i], " %s", words[i & 3]);

    }

    =============

    I get some AMAZING speed differences.

    In this test code strjoin consumes 250ms and concatenation 20940ms.

    The strjoin vs concatenation ratio becomes 1,2%, in favor of

    strjoin!!!

    Am I doing or measuring something totally wrong?

     

    Kim

     

    That's very interesting.

    It took me a while to figure out where the huge time difference was coming

    from.

     

    The answer is the difference in time it takes Eagle to fetch a string

    compared to an array element.

     

    string a[] = {"test"};

    string b = "test";

     

    runtext += b;

    runtext += a[0];

     

    These run at very different speeds.

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • k.portman
    0 k.portman over 13 years ago in reply to autodeskguest

    Il 24/06/2013 02:30, Warren Brayshaw ha scritto:

    I timed it again using a Win7 32bit Dual Core mailto:T6670@2.20GHz

     

    On the first pass the strJoin was 82% of the Concatenation time

     

    Subsequent passes averaged 65% of the Concatenation time and quite

    consistant.

     

    So although strJoin took longer on the first pass it was always faster than

    concatenation.

     

    Hi Warren,

     

    First, thanks for writing the test ULP to time the 2 solutions!

    I can confirm your results, the first run gives 91% and second 73% speed

    between strjoin vs concatenation. With 100.000 loops I get times on the

    order of 60 to 70ms, running on Core2-Duo 3.16GHz Win-7/64bit.

     

    Now, I suggest to broaden the test cases a little bit, here's why:

    Often there is a need to build more complex commands, using sprintf.

    On some system ULPs I can see code like this:

    =============

    string Cmd, h;

    sprintf(h, "EDIT %s.PaC;\nGRID %s;\n", s[0], Unit);

    Cmd += h;

    =============

     

    In this kind of cases sprintf() formatting becomes beneficial, else you

    have to write something like following (hardly readable):

    =============

    Cmd = "EDIT "s[0]".PaC;\nGRID "Unit+";\n";

    =============

     

    If I modify your test ULP inside the loops like this:

    =============

    for(i=1; i<100000; i++){

         string s;

         sprintf(s, " %s", words[i & 3]);

         runtext += s;

    }

     

    for(i=1; i<100000; i++){

         sprintf(a[i], " %s", words[i & 3]);

    }

    =============

    I get some AMAZING speed differences.

    In this test code strjoin consumes 250ms and concatenation 20940ms. The

    strjoin vs concatenation ratio becomes 1,2%, in favor of strjoin!!!

    Am I doing or measuring something totally wrong?

     

    Kim

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to dukepro

    Chuck Huber wrote on Sun, 23 June 2013 05:52

    Interesting,

     

    I consistently get results showing that strjoin() is about twice as

    fast

    as the concatenate.  This is on a 3GHz Pentium running Linux 2.6.34.

    But as you mentioned, it's miniscule compared to the time it takes to

    execute the script.

     

     

     

    Hi Chuck

     

    My previously mentioned times were from a P500 running Win2000. I use that

    PC for writing the ULP as it shows up bad coding choices. If it's fast on

    that machine then its acceptable.

     

     

    I timed it again using a Win7 32bit Dual Core mailto:T6670@2.20GHz

     

    On the first pass the strJoin was 82% of the Concatenation time

     

    Subsequent passes averaged 65% of the Concatenation time and quite

    consistant.

     

    So although strJoin took longer on the first pass it was always faster than

    concatenation.

     

    Warren

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to dukepro

    Hi Chuck

     

    My previously mentioned times were from a P500 running Win2000. I use that

    PC for writing the ULP as it shows up bad coding choices. If it's fast on

    that machine then its acceptable.

     

     

    I timed it again using a Win7 32bit Dual Core mailto:T6670@2.20GHz

     

    On the first pass the strJoin was 82% of the Concatenation time

     

    Subsequent passes averaged 65% of the Concatenation time and quite

    consistant.

     

    So although strJoin took longer on the first pass it was always faster than

    concatenation.

     

    Warren

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 13 years ago in reply to autodeskguest

    Interesting,

     

    I consistently get results showing that strjoin() is about twice as fast

    as the concatenate.  This is on a 3GHz Pentium running Linux 2.6.34.

    But as you mentioned, it's miniscule compared to the time it takes to

    execute the script.

     

    See attached screen shot.

     

        - Chuck

     

    On 06/22/2013 03:37 AM, Warren Brayshaw wrote:

    Hi

     

    It appears there is no real speed advantage using the array/string join

    method in Eagle ULP. The method is used in other coding to advantage. It is

    said that many browsers have optimised their treatment of string

    concatenation and have it running faster than array/string join.

     

    I got curious to see what the advantage gain was in Eagle. Run the attached

    ULP that times the two methods. The first time its run there is no

    difference in time between the two methods but run it again (Go) and you

    see concatenation take the same time but array/string gets quicker. I

    suspect the array is still in place so the ULP processor does not need to

    create it. Normally a ULP would build the exit(command string) only once so

    both methods are as quick as each other.

     

    I feel the advantage of running a script is that Eagle appears to perform

    the commands from the script far faster than it processes the commands in

    an exit command and advantages like speed of rendering the result in the

    editor. You can see the difference on slower PCs. You can see from the ULP

    that saving the text string (from the concatenation test) only adds a few

    milliseconds so for me its often the preferred technique.

     

    Enjoy

     

    Warren

     

     

     

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>