EAGLE User Support (English) Pin's Numbers are missing
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 434 views
  • Users 0 members are here
Related

Pin's Numbers are missing

autodeskguest
autodeskguest over 17 years ago

Hello,

 

I am creating a new library device based on the TSSOP16 package which I got from the "ref-packages.lbr" library.  For some reason the pin numbers of the device are not shown and only the symbol labels are shown.

 

There is another device in the library "texas-msp.lbr" which uses the TSSOP-16 package, the device is MAX3221-TSSOP16, and it has the same problem.

 

Any idea why is that and how can solve it.

 

Thanks

EitanB

 

Attachments:
3487.att1.html.zip
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Hello,

     

    The problem was with the visible, i.e. one of the pins was off.  I wonder if

    there is not way to set the visible to the whole symbol?

     

    Thanks

    Eitan

     

     

    "Eitan Barazani" <eitanbarazani@gmail.com> wrote in message

    news:ge358q$irh$1@cheetah.cadsoft.de...

    Hello,

     

    Sorry this was not the problem.

     

    Thanks,

    EitanB

     

    "Richard Herman" <postbus@het-audio-team.removethis.nl> wrote in message

    news:ge1l35$the$1@cheetah.cadsoft.de...

    Eitan Barazani schreef:

    Hello,

    I am creating a new library device based on the TSSOP16 package which I

    got from the "ref-packages.lbr" library.  For some reason the pin

    numbers of the device are not shown and only the symbol labels are

    shown.

    There is another device in the library "texas-msp.lbr" which uses the

    TSSOP-16 package, the device is MAX3221-TSSOP16, and it has the same

    problem.

    Any idea why is that and how can solve it.

    Thanks

    EitanB

     

     

    Hello Eitan,

     

    While designing the symbol for your device, click the 'change' icon and

    select 'visible'. choices are: Off,Pin,Pad,Both.

     

    HTH,

     

    Richard

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Hello,

     

    The problem was with the visible, i.e. one of the pins was off.  I wonder if

    there is not way to set the visible to the whole symbol?

     

    Thanks

    Eitan

     

     

    "Eitan Barazani" <eitanbarazani@gmail.com> wrote in message

    news:ge358q$irh$1@cheetah.cadsoft.de...

    Hello,

     

    Sorry this was not the problem.

     

    Thanks,

    EitanB

     

    "Richard Herman" <postbus@het-audio-team.removethis.nl> wrote in message

    news:ge1l35$the$1@cheetah.cadsoft.de...

    Eitan Barazani schreef:

    Hello,

    I am creating a new library device based on the TSSOP16 package which I

    got from the "ref-packages.lbr" library.  For some reason the pin

    numbers of the device are not shown and only the symbol labels are

    shown.

    There is another device in the library "texas-msp.lbr" which uses the

    TSSOP-16 package, the device is MAX3221-TSSOP16, and it has the same

    problem.

    Any idea why is that and how can solve it.

    Thanks

    EitanB

     

     

    Hello Eitan,

     

    While designing the symbol for your device, click the 'change' icon and

    select 'visible'. choices are: Off,Pin,Pad,Both.

     

    HTH,

     

    Richard