EAGLE User Support (English) Pin's Numbers are missing
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 424 views
  • Users 0 members are here
Related

Pin's Numbers are missing

autodeskguest
autodeskguest over 17 years ago

Hello,

 

I am creating a new library device based on the TSSOP16 package which I got from the "ref-packages.lbr" library.  For some reason the pin numbers of the device are not shown and only the symbol labels are shown.

 

There is another device in the library "texas-msp.lbr" which uses the TSSOP-16 package, the device is MAX3221-TSSOP16, and it has the same problem.

 

Any idea why is that and how can solve it.

 

Thanks

EitanB

 

Attachments:
3487.att1.html.zip
  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Eitan Barazani schrieb:

    Hello,

     

    I am creating a new library device based on the TSSOP16 package which

    I got from the "ref-packages.lbr" library.  For some reason the pin

    numbers of the device are not shown and only the symbol labels are

    shown.

     

    I am not sure what you want to tell us.

    Are you writing about the pad names that are not visible?

    If this is true, try

      SET PAD ON | OFF

    in the command line or click Options/Set/Misc: Display Pad Names

     

    HTH

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Eitan Barazani schrieb:

    Hello,

     

    I am creating a new library device based on the TSSOP16 package which

    I got from the "ref-packages.lbr" library.  For some reason the pin

    numbers of the device are not shown and only the symbol labels are

    shown.

     

    I am not sure what you want to tell us.

    Are you writing about the pad names that are not visible?

    If this is true, try

      SET PAD ON | OFF

    in the command line or click Options/Set/Misc: Display Pad Names

     

    HTH

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm