EAGLE User Support (English) Wire width in Eagle layout editor
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
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 2228 views
  • Users 0 members are here
Related

Wire width in Eagle layout editor

av8or1
av8or1 over 12 years ago

I have been using the free version of Eagle for evaluation for a couple of weeks now.  Although as a software engineer I am disturbed by how freqently Eagle crashes without any recovery, I decided to support the product and bought a license.  While working with the free version the wire widths that I had in my design were shown in what I presume were inches.  The wire widths were:

 

0.254 0.3048 0.4064 0.6096 0.8128 1.016 1.27 1.4224 1.6764 1.778 etc.

 

But now when I right-click on a wire and left-click on Properties, I see the values in what appear to be mm:

 

0 0.01 0.012 0.016 0.024 0.032 0.04

 

The wires don't appear to have changed really of course, and these numbers are equivalent.  However, I want to go back to the other unit system.  I have searched the help docs within Eagle, online and played around with options and such for a couple of hours now.  Cannot figure out how to change it back.

 

So the question is: how can I do this?

 

Thanks!

 

 

  • Sign in to reply
  • Cancel
Parents
  • av8or1
    0 av8or1 over 12 years ago

    Thanks. Yeah I tried that but it doesn't do anything. Only affects the dimension tool.  What is odd is that I have another board in the same project but yet this behavior doesn't repeat when I edit that board,  and I can do it without restarting eagle!  Strange!

     

    Anyway. Thanks again. Maybe something will break in the next couple of days.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • av8or1
    0 av8or1 over 12 years ago

    Thanks. Yeah I tried that but it doesn't do anything. Only affects the dimension tool.  What is odd is that I have another board in the same project but yet this behavior doesn't repeat when I edit that board,  and I can do it without restarting eagle!  Strange!

     

    Anyway. Thanks again. Maybe something will break in the next couple of days.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 12 years ago in reply to av8or1

    Hi,

     

    See screenshots:

    image

     

    image

     

    (Or you can just type grid on the command area, and the same window will pop up).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • av8or1
    0 av8or1 over 12 years ago in reply to shabaz

    Yup, you are correct. I played around enough today until I figured it out. Thank you for the reply!