EAGLE User Support (English) Gerber exports padding around board outline
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 181 subscribers
  • Views 472 views
  • Users 0 members are here
Related

Gerber exports padding around board outline

qwertymodo
qwertymodo over 12 years ago

I have a board design that I have been trying to export as a Gerber, but every time I do, the Gerber outline is larger than it's supposed to be.  I know that silkscreen or other items outside the board dimensions will do this, but I've confirmed that this isn't the case.  Here is the board in Eagle (6.5), with all layers enabled, so you can see that nothing is outside of the board outline:

 

image

 

Eagle automatically cropped the image because there was nothing outside of that area.  Now, when I export the Gerber files, this is what I get:

 

image

 

The padding on the left and right appears in every Gerber viewer I've used, so it's definitely in the file, not just a rendering error on OSHPark's end.  After some messing around, I've confirmed that it's due to the QFP footprint and that it only occurs when it is rotated 45 degrees like that.  I made that footprint myself, and it is only SMD pads, no labels, no keepout, just the pads.  So why is the Gerber export so badly screwing up the board outline?  It only does it for the top layer, the bottom layer is the correct size.  Any thoughts?

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 12 years ago

    On 09/10/2013 10:06 PM, Ben Whitman wrote:

    I have a board design that I have been trying to export as a Gerber, but

    every time I do, the Gerber outline is larger than it's supposed to be.

    ...

     

    After some messing around, I've confirmed that it's due

    to the QFP footprint and that it only occurs when it is rotated 45

    degrees like that.  I made that footprint myself, and it is only SMD

    pads, no labels, no keepout, just the pads.

     

    Hmmm... Interesting.

     

    Have you tried a "display all".  On the guess hat there's some artifact

    in the package, that may help find it.

     

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 12 years ago

    On 09/10/2013 10:06 PM, Ben Whitman wrote:

    I have a board design that I have been trying to export as a Gerber, but

    every time I do, the Gerber outline is larger than it's supposed to be.

    ...

     

    After some messing around, I've confirmed that it's due

    to the QFP footprint and that it only occurs when it is rotated 45

    degrees like that.  I made that footprint myself, and it is only SMD

    pads, no labels, no keepout, just the pads.

     

    Hmmm... Interesting.

     

    Have you tried a "display all".  On the guess hat there's some artifact

    in the package, that may help find it.

     

        - Chuck