EAGLE User Support (English) why the odd sizes?
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 179 subscribers
  • Views 365 views
  • Users 0 members are here
Related

why the odd sizes?

fritzz
fritzz over 12 years ago

The deault sizes for text width in the menu are 12 16 24 32 40 50 56 etc mil

 

Why does Eagle use these as the default? Why not use 10 15 20 25 30 etc mil??

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 29/09/13 02:32, d r wrote:

    The deault sizes for text width in the menu are 12 16 24 32 40 50 56 etc

    mil

     

    Why does Eagle use these as the default? Why not use 10 15 20 25 30 etc

    mil??

     

    Perhaps because 4thou ("mil") is very close to 0.1mm?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 29/09/13 02:32, d r wrote:

    The deault sizes for text width in the menu are 12 16 24 32 40 50 56 etc

    mil

     

    Why does Eagle use these as the default? Why not use 10 15 20 25 30 etc

    mil??

     

    Perhaps because 4thou ("mil") is very close to 0.1mm?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fritzz
    0 fritzz over 12 years ago in reply to autodeskguest

    Why the 12 16 24 32?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to fritzz

    As the sizes would roughly correspond as following:

     

    12 thou ~ 0.3mm

    16 thou ~ 0.4mm

    24 thou ~ 0.6mm

    32 thou ~ 0.8mm

     

    Dave.