EAGLE User Support (English) Has anyone written a ULP for assisting in pad renaming?
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 179 subscribers
  • Views 539 views
  • Users 0 members are here
  • rename
  • pad
  • ulp
Related

Has anyone written a ULP for assisting in pad renaming?

Eriond
Eriond over 12 years ago

I'm currently making a DDR3 package, and quickly realized that it's no fun manually renaming all 204 pads.

What I'm looking for is a ULP that could assist me in this tedious task.

Ideally, I'd like it to have a simple dialog asking just two things: Seed and Increment. Both being integer values, with the option to enter a negative increment.

After entering both values, I would start cklicking/selecting the pads, one at a time. For each successful selection, the pad would be renamed and the next incremented value would be shown somewhere (maybe in the status field at the bottom?) This would continue until I manually abort the ULP in some way.

 

Has such a tool already been conceived, or is it maybe part of some more extensive toolset?

If not, I would be eternally grateful if someone with skills in ULP could take the time to write this tool. I myself have browsed through the ULP manual, but couldn't quite understand how mouse input could be captured by the ULP...

 

Kind regards

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Eriond,

     

    I don't know ULP, but as a suggestion, you could write a program/script to just generate EAGLE commands that create the pads with the correct name, all in one.

    For example, a script containing this line:

    smd 0.5 1.5 '1' (4.0 5.0)

    would create an SMD pad of dimensions 0.5x1.5 at location (4 5) with the name '1'.

     

    Normally for any package of greater than (say) 16 pins, it may be easier to write a program that generates a script for you, rather than load and edit a package manually with mouse-clicks.

     

    Probably there is a script command to rename pads, but the above works well for me so I've not searched for an alternative.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to shabaz

    On 12/11/13 22:24, shabaz wrote:

    Hi Eriond,

     

    I don't know ULP, but as a suggestion, you could write a program/script

    to just generate EAGLE commands that create the pads with the correct

    name, all in one.

     

    I second this suggestion. When generating packages, or indeed whole

    libraries in the case of connector families, my normal approach is to

    hack some Python to write a SCR file to make the library parts.

     

    Other scripting languages are also available image

     

    Cheers,

    Rob

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to shabaz

    On 12/11/13 22:24, shabaz wrote:

    Hi Eriond,

     

    I don't know ULP, but as a suggestion, you could write a program/script

    to just generate EAGLE commands that create the pads with the correct

    name, all in one.

     

    I second this suggestion. When generating packages, or indeed whole

    libraries in the case of connector families, my normal approach is to

    hack some Python to write a SCR file to make the library parts.

     

    Other scripting languages are also available image

     

    Cheers,

    Rob