EAGLE User Support (English) Has anyone written a ULP for assisting in pad renaming?
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 179 subscribers
  • Views 543 views
  • Users 0 members are here
  • rename
  • pad
  • ulp
Related

Has anyone written a ULP for assisting in pad renaming?

Eriond
Eriond over 12 years ago

I'm currently making a DDR3 package, and quickly realized that it's no fun manually renaming all 204 pads.

What I'm looking for is a ULP that could assist me in this tedious task.

Ideally, I'd like it to have a simple dialog asking just two things: Seed and Increment. Both being integer values, with the option to enter a negative increment.

After entering both values, I would start cklicking/selecting the pads, one at a time. For each successful selection, the pad would be renamed and the next incremented value would be shown somewhere (maybe in the status field at the bottom?) This would continue until I manually abort the ULP in some way.

 

Has such a tool already been conceived, or is it maybe part of some more extensive toolset?

If not, I would be eternally grateful if someone with skills in ULP could take the time to write this tool. I myself have browsed through the ULP manual, but couldn't quite understand how mouse input could be captured by the ULP...

 

Kind regards

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 13/11/2013 10:28 a.m., Eriond wrote:

    I'm currently making a DDR3 package, and quickly realized that it's no

    fun manually renaming all 204 pads.

    What I'm looking for is a ULP that could assist me in this tedious task.

     

     

    What you likely need to have done is create the first SMD with a command

    like SMD 50 50 -100 '1' (See help SMD)

     

    That makes a  pad named 1 and then subsequent SMD are named sequentially

    2,3,4 etc instead of the default P$1 P$2 etc.

     

    Rather than create a ULP it would be faster to rename the pads. Dont use

    the information "i" icon but rather the 'Name' icon which is much faster.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 13/11/2013 10:28 a.m., Eriond wrote:

    I'm currently making a DDR3 package, and quickly realized that it's no

    fun manually renaming all 204 pads.

    What I'm looking for is a ULP that could assist me in this tedious task.

     

     

    What you likely need to have done is create the first SMD with a command

    like SMD 50 50 -100 '1' (See help SMD)

     

    That makes a  pad named 1 and then subsequent SMD are named sequentially

    2,3,4 etc instead of the default P$1 P$2 etc.

     

    Rather than create a ULP it would be faster to rename the pads. Dont use

    the information "i" icon but rather the 'Name' icon which is much faster.

     

    HTH

    Warren