EAGLE User Support (English) How do I create a solder resist pattern in Eagle?
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
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 1348 views
  • Users 0 members are here
  • mask
  • resist
  • solder
Related

How do I create a solder resist pattern in Eagle?

billpenner
billpenner over 12 years ago

I have used photoshop to create a mask from the eagle print but it is tedious. There must be something I am missing in Eagle such as a ULP that would make it easier. Can anyone help me>

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 23/11/13 19:18, billpenner wrote:

    I have used photoshop to create a mask from the eagle print but it is

    tedious. There must be something I am missing in Eagle such as a ULP

    that would make it easier. Can anyone help me>

     

     

    Do you mean "how can I export the tStop and bStop layers?" or would that

    get a "the what?" answer?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billpenner
    0 billpenner over 12 years ago in reply to autodeskguest

    Thanks for the help. I can print the Stop pattern but It is negative, that is I will have to make a transparency then make a photo film negative of that for a mask to the board. I am making the layouts, film positives, negatives then using dry film resist to make the PC boards and solder masks I am trying to eliminate some of the steps. I would like to eliminate all of the lithographic processes if possible. I don't require all that much precision. Its only a hobby for me. I think if I could get a negative output from Eagle it be an answer.

    Thanks

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 12 years ago in reply to billpenner

    On 11/23/2013 05:06 PM, billpenner wrote:

    Thanks for the help. I can print the Stop pattern but It is negative,

    that is I will have to make a transparency then make a photo film

    negative of that for a mask to the board. I am making the layouts, film

    positives, negatives then using dry film resist to make the PC boards

    and solder masks I am trying to eliminate some of the steps. I would

    like to eliminate all of the lithographic processes if possible.

     

    Bill,

     

    To my knowledge, Eagle can not produce a negative Gerber file.  So

    you're left to external tools to do so.

     

    Maybe this will help:

     

     

    • In Eagle, setup the CAM section normally to emit GERBER_RS274X and

        process the section to produce the desired Gerber file.  For the top

        layer, include only the tStop layer, and the Dimension layer for

        alignment.  For the bottom layer, use bStop and Dimension and be

        sure to mirror the layer.

     

    • Using gerbv to view the Gerber file:

          o Set the layer color to pure white (#FFFFFF).

          o Click-right on the layer and choose "Invert Layer Color"

          o Print the layer.

     

    HTH,

        - Chuck

     

     

    Attachments:
    2538.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • billpenner
    0 billpenner over 12 years ago in reply to dukepro

    Thank you very much. I now know to search elsewhere. I guess the litho is not bad after all. will try the gerbv also.

    Thanks again

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billpenner
    0 billpenner over 12 years ago in reply to dukepro

    Thank you very much. I now know to search elsewhere. I guess the litho is not bad after all. will try the gerbv also.

    Thanks again

    Bill
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.