EAGLE User Support (English) OSX: system("pwd > zzzTempFile"); does not create zzzTempFile
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
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 412 views
  • Users 0 members are here
Related

OSX: system("pwd > zzzTempFile"); does not create zzzTempFile

zelisse
zelisse over 12 years ago

I want to know the current home directory on a Macintosh running Mavericks.

 

I'm using in an .ulp

 

system("pwd > zzzTempFile");

 

but unfortunately it does not create the zzzTempFile. Running the same command in the Terminal works fine.


What should I do to execute system commands and store the results in a (tempory) file?

 

Thanks for your time & help.

 

Karel

  • Sign in to reply
  • Cancel
  • AnalogNotes
    0 AnalogNotes over 12 years ago

    Just a guess, but the file is probably being created, but not where you expect.

     

    Put a full path in front of the zzzTempFile name to make sure it is where you want it to be.  I don't know if Mavericks is the same as the older stuff (I'm running 10.5.8) but on my system I would use:

     

    pwd > /Users/doug/Desktop/zzzTempFile

     

    Regards,

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • zelisse
    0 zelisse over 12 years ago in reply to AnalogNotes

    Thanks Doug for your reply.

     

    The reason I want to export the home directory is that I can then read it back and use it in the .ulp. Something like this:

     

             string tempFileName = "zzzTempFile";

        string completeCommand = "pwd  > " + tempFileName;

        system( completeCommand );

        string lines[];

        fileread( lines, tempFileName );

        string removeTempFile = "rm " + tempFileName;

        system( removeTempFile );

        string homeDirectory =  lines[0];

     

    It always fails the 'fileread( lines, tempFileName);' So maybe the output is in an unexpected location, the fileread does not look in the same unexpected location.

     

    On mavericks the full path—as you suggested—works, system( "pwd `/zzzTempFile") does not.

     

    The only way round it—as far as I can see—is to call an external, for example python, program which does it all. But that means yet another snippet of code.

     

    I presume that failing system("pwd zzzTempFile") is a bug.

     

    The real issue is that system() cannot return anything apart from whether the operation was successful or not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • AnalogNotes
    0 AnalogNotes over 12 years ago in reply to zelisse

    I do this kind of thing a lot actually.  Since I have different designs, I always put my engineering notes and temporary files in the same directory with the schematic and board files that I'm working on.  There is a brief discussion of this at: http://www.element14.com/community/thread/26510/l/engineering-notes-within-eagle

     

    I use this general idea in all my scripts that write something to disk, and I think you might be able to modify it for your needs:

    string ScriptName = "my-script";

    string Version = "1.00";

     

    string a[];

    string command;

    string scriptfile;

     

     

     

    if (schematic) {

      schematic(SCH){

        string directory = filedir(SCH.name) + "scripts";

        int n = fileglob(a, directory);

        if (n == 0){

          sprintf(command, "mkdir %s", directory);

          system(command);

        }

        int t = time();

        string datestring = t2string(t, "yyyyMMdd-hh:mm:ss");

        sprintf(scriptfile, "%s/%s-%s.scr", directory, ScriptName, datestring);

        output(scriptfile) {

          printf("Do something here....\n");

        }

      }

      sprintf(command, "script %s", scriptfile);

      exit(command);

    }

    (Change as appropriate to use board instead of schematic.)  This script creates a subdirectory in your project called "scripts" and puts everything there to keep from cluttering things up.  I don't delete files, in case I want to go back and see what I really did or do some debugging, so I add a date string into the filename to keep them unique.  For your purposes, I haven't included a read statement, but you should be able to just use "scriptfile".

     

    FWIW, I used to create command strings in memory and run them on exit, but I seem to write long scripts and I keep using up the memory buffers, so that's what inspired me to write scripts to disk and run them from there.