EAGLE User Support (English) Demo2.sch, Q1 value not is displayed.  How do I correct this?
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 259 views
  • Users 0 members are here
Related

Demo2.sch, Q1 value not is displayed.  How do I correct this?

Former Member
Former Member over 12 years ago

Software download:  Eagle 6.5.0.

When ERC is run, there are 3 warnings. 2 are easily ignored. The third is that Q1's value is missing. This is easily corrected. The problem is that the value does not display, eg. 1n4148 for D1, or 24.0000MHz for q1.  How do I get the value for Q1 to display?

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 12/12/2013 6:40 p.m., m farb wrote:

    Software download:  Eagle 6.5.0.

    When ERC is run, there are 3 warnings. 2 are easily ignored. The third

    is that Q1's value is missing. This is easily corrected. The problem is

    that the value does not display, eg. 1n4148 for D1, or 24.0000MHz for

    q1.  How do I get the value for Q1 to display?

     

     

    The value of Q1 is not displayed because previously Q1 was smashed and

    the the value was deleted.(not really deleted, just not displayed any more)

     

    To get it back, select SMASH, hold down the SHIFT key and click on Q1.

    The value will reappear.

     

    See the HELP > smash

     

    HTH

     

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to autodeskguest

    Thank you. That works.

     

    -m