EAGLE User Support (English) Libraries invisible from schematic
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
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 547 views
  • Users 0 members are here
Related

Libraries invisible from schematic

Former Member
Former Member over 12 years ago

Hi I'm running Ubuntu 10.04 and installed eagle 5.7.0-2 via pkg mgr. Problem is while libraries are visible in eagleroot they cannot be found from ADD in a schematic. I've deleted/re-installed several times with no joy. Including (initially from a tar file) Any ideas gratefully rxd

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    Am 13.12.2013 11:41, schrieb Bill Rees:

    Hi I'm running Ubuntu 10.04 and installed eagle 5.7.0-2 via pkg mgr.

    Problem is while libraries are visible in eagleroot they cannot be found

    from ADD in a schematic. I've deleted/re-installed several times with no

    joy. Including (initially from a tar file) Any ideas gratefully rxd

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/97135

     

     

    Please try two commands in the command line for example in the

    Schematic Editor:

     

       USE -*

    then

       USE *

     

    Now all library files should be available in the ADD dialog.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to autodeskguest

    Thanks to Richard. That solved the problem instantly!!!!

    Regards

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to autodeskguest

    Thanks Richard.

    Regards

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 13/12/2013 11:41 p.m., Bill Rees wrote:

    Hi I'm running Ubuntu 10.04 and installed eagle 5.7.0-2 via pkg mgr.

    ...................

     

     

    Hi Bill

     

    v5.7 was particularly troublesome. If you are going to use v5 for some

    time I suggest you update to the last v5  at

    ftp://ftp.cadsoft.de/eagle/program/5.12/

     

    HTH

    Warren