Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) GND & VCC pin on IC
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 1883 views
  • Users 0 members are here
Related

GND & VCC pin on IC

e14 Contributor
e14 Contributor over 12 years ago

This is for most of you probably the most obvious thing in designing.............. but I as a newbee have this question :

 

I take a LM 1458 from the library onto the schematic, I select both opamps, and start connecting........ but there is no VCC or GND, (although they are drawn in the library drawing) I have named the plus and minus leads of the circuit VCC and GND nothing , also in info on the 1458 is no mention of vcc or gnd, even in the help I could not find a hint

then in the board is also no airwire to one of both pins?????

 

What is the "golden grip" that I have missed? 

 

Jack

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 16/12/13 21:16, jack asnack wrote:

    This is for most of you probably the most obvious thing in

    designing.............. but I as a newbee have this question :

     

    It is a very common newbie question.

     

     

    I take a LM 1458 from the library onto the schematic, I select both

    opamps, and start connecting........ but there is no VCC or GND,

    (although they are drawn in the library drawing)

     

    No, they're not. The pins you see on the control panel are called 'V+'

    and 'V-'

     

    I have named the plus

    and minus leads of the circuit VCC and GND nothing , also in info on the

    1458 is no mention of vcc or gnd, even in the help I could not find a

    hint

     

    No, as I said, they're not called that.

     

    then in the board is also no airwire to one of both pins?????

     

    What is the "golden grip" that I have missed? 

     

    Two things.

     

    The pins are named V+ and V-, so to get Eagle's automatic power supply

    connection (which some people really dislike) you need to place supply

    symbols V+ and V- on your schematic.

     

    If you want to have the pins shown on the op-amp, as they appear in the

    library diagram, you need to use "invoke". Check the help for how to do

    that.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 16/12/13 21:16, jack asnack wrote:

    This is for most of you probably the most obvious thing in

    designing.............. but I as a newbee have this question :

     

    It is a very common newbie question.

     

     

    I take a LM 1458 from the library onto the schematic, I select both

    opamps, and start connecting........ but there is no VCC or GND,

    (although they are drawn in the library drawing)

     

    No, they're not. The pins you see on the control panel are called 'V+'

    and 'V-'

     

    I have named the plus

    and minus leads of the circuit VCC and GND nothing , also in info on the

    1458 is no mention of vcc or gnd, even in the help I could not find a

    hint

     

    No, as I said, they're not called that.

     

    then in the board is also no airwire to one of both pins?????

     

    What is the "golden grip" that I have missed? 

     

    Two things.

     

    The pins are named V+ and V-, so to get Eagle's automatic power supply

    connection (which some people really dislike) you need to place supply

    symbols V+ and V- on your schematic.

     

    If you want to have the pins shown on the op-amp, as they appear in the

    library diagram, you need to use "invoke". Check the help for how to do

    that.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    I have just made the changes and as you predicted this does the trick, thank you for showing me.

    Jack