I need an example of how to design a controlled impedance differential pair of pcb routes
using Cadsoft Eagle vsn 5.12.0.
I need an example of how to design a controlled impedance differential pair of pcb routes
using Cadsoft Eagle vsn 5.12.0.
James,
Sorry for the multiple sends, I keep hitting the wrong keys as I am typing.
Thanks for taking the time to answer. Since I posted the question
I saw a Altium example that shows both traces being routed simultaneously
after a minor amount of setup. I later found out that Eagle offers the same
thing in vsn 6. I am considering buying DipTrace for $895.00 since upgrade
to Eagle vsn 6 will cost me $549.00. I have been with Eagle for years but I
need to save $$$.
Regards,
Bankole
James,
Thanks for taking the time to explain. Since i posted my question
I saw an Altium example showing that both traces are simultaneously both traces that Eagle vsn 6
James,
Thanks for taking the time to answer. Since I posted the question
I saw a Altium example that shows both traces being routed simultaneously
after a minor amount of setup. I later found out that eagle offers the same thing in vsn 6.
Bankole Paris wrote on Mon, 13 January 2014 14:36
I need an example of how to design a controlled impedance differential
pair of pcb routes
using Cadsoft Eagle vsn 5.12.0.
--
To view any images and attachments in this post, visit:
In V5 and before, you have to do the routing manually. First, you need to
figure out what the trace width and separation should be (EAGLE will not
help you be an engineer). Then once you have that, what I do is figure out
what grid setting I need to get the separation exactly right when routing
that trace width. I do this by drawing a quick diagram and figuring out
center-to-center spacing of the traces. Then I usually set my grid to 1/2
of that and then route to make sure 2 grid spaces are between the diff pair
traces. Diagonals are different and if you really want exact then you need
to do some calculations and move them closer to each other.
The summary is EAGLE won't help you other than letting you put traces
exactly where you need them. So you have to do some low-level design work
to get these to work. I've done dozens of boards this way and they
function just fine.
Cheers,
James.
--
James Morrison ~~~ Stratford Digital
Specializing in CadSoft EAGLE
Online Sales to North America
Electronic Design Services
EAGLE Enterprise Toolkit
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.