EAGLE User Support (English) Eagle TQFN-Autorouter
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 238 views
  • Users 0 members are here
Related

Eagle TQFN-Autorouter

djm2
djm2 over 12 years ago

Hi there

 

I am using a PIC18F87K22 PIC in a TQFN-80 package in a design I am creating.  I created the part in a library and copied the TQFN footprint from another project.  Everything on my board will route with the autorouter apart from this part.  I tried manually routing a tiny section of wire from each of the pins out by a 1 or 2 mm and then tried the autorouter again then it worked.

 

The pads of the TQFN part are 0.3mm x 1.2mm and I set the grid of the PCB to 0.1mm and I also set the routing grid setting to 0.05mm and still cannot get it to auto route.  I know people will say why bother with the auto router just do it manually but I really want to use the autorouter.  I reduced the size of the net class down to 5mil still with no luck.  I have larger SMD parts - SOIC 16 and they auto route fine. 

 

Can anyone make any suggestions?

 

David

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 12 years ago

    Hi,

     

    maybe it is a matter if minimum clearance or net classe settings? What are the values there? Is it possible to connect without clearance errors?

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Richard_H
    0 Richard_H over 12 years ago

    Hi,

     

    maybe it is a matter if minimum clearance or net classe settings? What are the values there? Is it possible to connect without clearance errors?

     

    Regards,

    Richard