EAGLE User Support (English) Help for footprint (edge mounted connector)
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 183 subscribers
  • Views 1487 views
  • Users 0 members are here
Related

Help for footprint (edge mounted connector)

cgroen
cgroen over 12 years ago

Hello,

I'm doing my first few boards in Eagle, and so far everything is running perfectly (and will upgrade to the full version now) image

On a new board I'm trying to do I have two 6 pin connectors that I would like to mount on the edge of the board (horisontal). I'm having a hard time how to design that as a footprint. There needs to be to cutouts in the board and these should be plated. I have attached a picture of the connecotor and a picture of how it has been done in another product.

Any help out there ? This is the last thing I need to resolve before my board is being sent (I'm using PCB-POOL)

 

Thanks for any help (would even consider paying you for a ready made footprint that would do this if reasonable..)

 

 

image

image

  • Sign in to reply
  • Cancel
Parents
  • eduardodemier
    0 eduardodemier over 11 years ago

    Hi.

    I need to create a package for a popular SMA edge connector. Mine is Emerson-Johnson 142-0721-881 but there are second source types as Jibao e. a.

    See below.

    Copper has to reach the pcb edge and the edge has to be plated for  GND(lower pads at right & left).

    How can I define the package?

    Thanks.

    Eduardo

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • eduardodemier
    0 eduardodemier over 11 years ago

    Hi.

    I need to create a package for a popular SMA edge connector. Mine is Emerson-Johnson 142-0721-881 but there are second source types as Jibao e. a.

    See below.

    Copper has to reach the pcb edge and the edge has to be plated for  GND(lower pads at right & left).

    How can I define the package?

    Thanks.

    Eduardo

    imageimage