EAGLE User Support (English) SMD pads thermals
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 343 views
  • Users 0 members are here
Related

SMD pads thermals

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I'm having difficulties adjusting the width of the gap on SMD pads and also

on vias. Eagle only generates very thin lines from the pad to the supply

plane. I figured that the gap percentage and minimum/maximum values in the

Supply tab of the DRC would allow me to adjust this but it looks like it has

no effect. The other parameters in the Supply tab of the DRC do have a

visible effect...

 

thanks,

 

TH

 

 

 

  • Sign in to reply
  • Cancel
  • esilviu
    esilviu over 17 years ago

    pad is connected to the supply polygon with 1,2,3 or 4 wires (depending on

    situation), and the width of the wire is the same with the width of polygon.

     

    "gap" can be modified from DRC settings, Supply tab, "Thermal" option. (you

    must check "Restring" too)

     

    After modifying DRC settings, run a ratsnest

     

    "TH" <thorswill@hotmail.com> wrote in message

    news:gi9ql1$ltj$1@cheetah.cadsoft.de...

    Hi,

     

    I'm having difficulties adjusting the width of the gap on SMD pads and

    also on vias. Eagle only generates very thin lines from the pad to the

    supply plane. I figured that the gap percentage and minimum/maximum values

    in the Supply tab of the DRC would allow me to adjust this but it looks

    like it has no effect. The other parameters in the Supply tab of the DRC

    do have a visible effect...

     

    thanks,

     

    TH

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Aha! I'd set the width of the polygons to 0 hence the thin lines on the

    thermals. All is well now.

     

    Many thanks eSilviu!

     

    regards,

    TH

     

    "eSilviu" <Silviu.Epure@ugal.ro> wrote in message

    news:gia5vk$q8v$1@cheetah.cadsoft.de...

    pad is connected to the supply polygon with 1,2,3 or 4 wires (depending on

    situation), and the width of the wire is the same with the width of

    polygon.

     

    "gap" can be modified from DRC settings, Supply tab, "Thermal" option.

    (you must check "Restring" too)

     

    After modifying DRC settings, run a ratsnest

     

    "TH" <thorswill@hotmail.com> wrote in message

    news:gi9ql1$ltj$1@cheetah.cadsoft.de...

    Hi,

     

    I'm having difficulties adjusting the width of the gap on SMD pads and

    also on vias. Eagle only generates very thin lines from the pad to the

    supply plane. I figured that the gap percentage and minimum/maximum

    values in the Supply tab of the DRC would allow me to adjust this but it

    looks like it has no effect. The other parameters in the Supply tab of

    the DRC do have a visible effect...

     

    thanks,

     

    TH