EAGLE User Support (English) Need help with LTC3129 linear part
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 440 views
  • Users 0 members are here
  • ltc3129
  • ltspice
  • ulp
  • linear_technlogy
Related

Need help with LTC3129 linear part

Former Member
Former Member over 11 years ago

I am working on a circuit using the LTC3129 and would like to lay out a pcb using eagle.  Can someone either generate the library or give me some hints on how to generate using ulp?

 

Bill

  • Sign in to reply
  • Cancel
  • dukepro
    0 dukepro over 11 years ago

    On 02/03/2014 12:35 PM, zmrbill wrote:

    I am working on a circuit using the LTC3129 and would like to lay out a

    pcb using eagle.  Can someone either generate the library or give me

    some hints on how to generate using ulp?

     

    Good morning, Bill,

     

    A User Language Program is not the right tool to generate this part.

    All in all, it is a read-only environment and can not directly change

    anything in the schematic, board, or library editors.  That being said,

    it can exit the program passing a string argument as a parameter to

    exit() that contains a script to execute.  The script can do anything

    that you can type in the command text box.

     

    I took a quick look at the datasheet for the LTC3129.  The best place to

    start is in the library editor with a personal library opened.  It is

    recommended to avoid editing any of the libraries that came with the

    distribution - the changes will likely be overwritten by updates and

    upgrades.

     

    First, with the library editor open, create a new symbol that closely

    matches the block diagram on the first page of the datasheet.  Make sure

    that the pins you add have the proper direction.  PWR is for power and

    ground pins.  IN and OUT signify the direction of the flow of power or

    signal.  The ERC will warn you if you have more than one OUT on a net,

    or if a net contains one or more IN's without an OUT.  You can read more

    about the characteristics of each direction in the manual.

     

    Next, create a package that accommodates the footprint of the '3129.

    Page 2 of the datasheet shows that this part is offered in two different

    packages - a QFP and an MSOP.  A suitable package may exist in

    smd-ipc.lpr.  If you find one there, you can drag it from the control

    panel to the library editor to include it in your library.  Don't forget

    to add the center pad on the bottom of the chip.  Pages 26 and 27 of the

    datasheet has the recommended pad layouts.

     

    Finally, create a new device for the '3129.  Add the symbol you created

    in the first step, and the package you copied or created in the second

    step.  Use the CONNECT to connect the pins on the symbol to the pads on

    the package.

     

    Save the library.  Go back to your schematic and USE the library, then

    UPDATE the library.  At this point, you should be able to ADD the new

    part to your schematic.

     

    It is a good idea to know how to create your own parts.  While the

    libraries included in the distribution are extensive, they are far from

    complete, and at the rate new parts are being invented, they will never

    be complete.  Additionally, there is no guarantee for accuracy on any of

    the distribution libraries.  Always verify the package against the

    datasheet.  I have had boards fabricated on more than one occasion that

    wound up useless because I didn't check the layout.

     

    There is more information on this process in the user manual and in the

    tutorial.  Look in the doc/ directory below Eagle's installation directory.

     

    I hope this helps get you started.

     

    Regards,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to dukepro

    Hey thanks Chuck,  I will use your reply as a guide.

     

    I have been a long time user of Ltspice and the link between Eagle and Ltspice is what really attracted me.  I also need to ability to design PCB.

     

    Bill