I've gotten an EAGLE schematic/board files from a web site. Using
EAGLE v4.16r2, I've run DRC - no problems. I've run CAM and submitted
gerbers to FreeDFM.com - no problems. I've submitted the gerbers to
BatchPCB.com - PROBLEMS! I see the same problem if I use EAGLE v5.3.0
to create the gerbers.
BatchPCB's bot complains that there are many lines less than 8 mil.
Using GCPrevue to check the gerbers shows that ALL of the SMD pads are
made with ~6 mil lines, instead of rectanges! How do I fix this
baffling problem?
-Dave Pollum