EAGLE User Support (English) Multiple VDD or VSS pins
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 1066 views
  • Users 0 members are here
Related

Multiple VDD or VSS pins

Former Member
Former Member over 17 years ago

Well I at times am torn between creating a schematic symbol that is

logical (group pins together with similar functions) or physical (pins

laid out like the package/footprints).  Right now I am doing a physical

layout and the IC has two VDD and two VSS pins.  Of course EAGLE doesn't

allow the pins to have the same name and so I was wondering if there is

a way to do that.  Do others simply name it VDD1 and VDD2?

 

If I was to create the schematic symbol as logical with a single VDD and

single VSS, can multiple pads in the footprint be attached to one pin? 

I tried this before and believe I had trouble with it.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    On Tue, 23 Dec 2008 21:53:32 +0800, "Timothy D. Swieter"

    <timothy@brilldea.com> wrote:

     

    Well I at times am torn between creating a schematic symbol that is

    logical (group pins together with similar functions) or physical (pins

    laid out like the package/footprints).  Right now I am doing a physical

    layout and the IC has two VDD and two VSS pins.  Of course EAGLE doesn't

    allow the pins to have the same name and so I was wondering if there is

    a way to do that.  Do others simply name it VDD1 and VDD2?

     

    If I was to create the schematic symbol as logical with a single VDD and

    single VSS, can multiple pads in the footprint be attached to one pin? 

    I tried this before and believe I had trouble with it.

     

    In library, name the GND pins VSS@1 and VSS@2.  EAGLE will then call

    both pins VSS.  HELP PIN for more info.

     

    -Dave Pollum

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 17 years ago

    Dave wrote:

    On Tue, 23 Dec 2008 21:53:32 +0800, "Timothy D. Swieter"

    <timothy@brilldea.com> wrote:

     

     

    Well I at times am torn between creating a schematic symbol that is

    logical (group pins together with similar functions) or physical (pins

    laid out like the package/footprints).  Right now I am doing a physical

    layout and the IC has two VDD and two VSS pins.  Of course EAGLE doesn't

    allow the pins to have the same name and so I was wondering if there is

    a way to do that.  Do others simply name it VDD1 and VDD2?

     

    If I was to create the schematic symbol as logical with a single VDD and

    single VSS, can multiple pads in the footprint be attached to one pin? 

    I tried this before and believe I had trouble with it.

       

     

    In library, name the GND pins VSS@1 and VSS@2.  EAGLE will then call

    both pins VSS.  HELP PIN for more info.

     

    -Dave Pollum

     

     

    Thanks Dave, I learn something new about everyday with EAGLE!  I will

    try this out later today.