Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How do i get rid of the vias in my solder mask (layer 29 7 30 stop)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 528 views
  • Users 0 members are here
Related

How do i get rid of the vias in my solder mask (layer 29 7 30 stop)

jollybv
jollybv over 11 years ago

Hi guys

I'm new to Eagle and battling a bit with creating the Gerber files in particular the stop mask (layer 29 & 30) what is happening when i generate the stop mask it give me the vias and the pads on my solder mask how do i get rid of the vias in my solder mask??

 

Regards

Brian

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 11 years ago

    On 02/11/2014 01:21 AM, Brian Van Staden wrote:

    Hi guys

    I'm new to Eagle and battling a bit with creating the Gerber files in

    particular the stop mask (layer 29 & 30) what is happening when i

    generate the stop mask it give me the vias and the pads on my solder

    mask how do i get rid of the vias in my solder mask??

     

    Good morning, Brian,

     

    From the board editor, click on DRC => Masks => Limit.  This specifies

    the maximum sized smd/pad/via that gets covered with mask.  Such

    features larger than this value have the mask pulled back.

     

    In general, you want the mask pulled back from all holes (set Limit to

    0) that are not specifically filled with a material.  The reason for

    this is that covering the hole creates an air pocket.  When the board

    goes through re-flow, the mask softens and the contained air will heat

    up and expand, possibly dislodging a nearby part.  One should also

    consider the application's environment and whether the board will

    operate at STP, or if it will be exposed to high  (i.e. submersion) or

    low ambient pressures (i.e. high altitude or space).

     

    There may be a compelling reason to cover smaller holes, but I can't

    think of any at the moment.

     

    The bottom line is that it's a design decision.

     

    HTH,

        - Chuck

     

     

    Regards

    Brian

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/103406

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jollybv
    0 jollybv over 11 years ago in reply to dukepro

    Hi Chuck

     

    Thanks for the reply I checked to see in the DRC - mask - limits, and it is set to 0 what i red there was that that " stop masks are generated for smds, pads and those vias that have a drill diameter that exceeds limits"  i have tried to check and see where i can change the vias drill size but not sure where, everything is set to default.

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jollybv
    0 jollybv over 11 years ago in reply to dukepro

    Hi Chuck

     

    Thanks for the reply I checked to see in the DRC - mask - limits, and it is set to 0 what i red there was that that " stop masks are generated for smds, pads and those vias that have a drill diameter that exceeds limits"  i have tried to check and see where i can change the vias drill size but not sure where, everything is set to default.

     

    Brian