EAGLE User Support (English) How can I add a ground plane?
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
  • Replies 5 replies
  • Subscribers 177 subscribers
  • Views 541 views
  • Users 0 members are here
Related

How can I add a ground plane?

autodeskguest
autodeskguest over 17 years ago

I am working on a 2 layer board. Should I be using a ground

plane, and if so how do I add it and perform auto routing?

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    On Tue, 23 Dec 2008 15:19:59 -0000, <basicbrd@noreply.co.uk> wrote:

     

    I am working on a 2 layer board. Should I be using a ground

    plane, and if so how do I add it and perform auto routing?

     

     

    Use the POLYGON command to create a copper pour.  This can be almost

    any shape you can think of.  IOW, it doesn't need to be a rectangle.

    Then use the NAME command to name the polygon GND.

    Note: The default line width of 16 mil (0.016") usually works well.

    However, if you have gaps in the pour, say between pads, then decrease

    the line width.  If you make the line width too narrow, you will

    create a huge Gerber file.

     

    -Dave Pollum

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    Hello, thank you for your reply, I am trying to understand this,

    can you clarify some points,

     

    what is a "copper pour" , is it on eagle 4 or 5?

    do I add the ground layer around my components or over the entire area?

    can I perform routing on the ground plane as well or only on the other

    layer?

    if yes, how do I route over the ground, as the routes need to cut space

    around them?

    tia.

    --

    "Dave" <dave@x.com> wrote in message

    news:0822l45msfhqis4vba9cnooefpmgd5p9t2@4ax.com...

    On Tue, 23 Dec 2008 15:19:59 -0000, <basicbrd@noreply.co.uk> wrote:

     

    >I am working on a 2 layer board. Should I be using a ground

    >plane, and if so how do I add it and perform auto routing?

     

    Use the POLYGON command to create a copper pour.  This can be almost

    any shape you can think of.  IOW, it doesn't need to be a rectangle.

    Then use the NAME command to name the polygon GND.

    Note: The default line width of 16 mil (0.016") usually works well.

    However, if you have gaps in the pour, say between pads, then decrease

    the line width.  If you make the line width too narrow, you will

    create a huge Gerber file.

     

    -Dave Pollum

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Hello, thank you for your reply, I am trying to understand this,

    can you clarify some points,

     

    what is a "copper pour" , is it on eagle 4 or 5?

    do I add the ground layer around my components or over the entire area?

    can I perform routing on the ground plane as well or only on the other

    layer?

    if yes, how do I route over the ground, as the routes need to cut space

    around them?

    tia.

    --

     

    Groundplanes aka. copper pours work in all Eagle versions,

    one way to make one is to type 'polygon gnd' and draw the outer edges of the groundplane to be.

    Before drawing you may also select stuff like width, hatch or solid, via thermals on/off etc.

     

    You can put groundplanes where you see fit, around the entire board or just in selected areas.

    When you then click ratsnest the pour is drawn, and automatically avoids routed tracks,

    and 'isolate' sets the isolation distance between tracks and pour.

     

    //Greg-

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    You can route on the plane too after it is "poured". As long as isolate is

    set, clicking ratsnest again will redraw the plane with proper spacing

    between the route and the rest of the plane.

     

    <basicbrd@noreply.co.uk> wrote in message

    news:gj5dsn$uav$1@cheetah.cadsoft.de...

    Hello, thank you for your reply, I am trying to understand this,

    can you clarify some points,

     

    what is a "copper pour" , is it on eagle 4 or 5?

    do I add the ground layer around my components or over the entire area?

    can I perform routing on the ground plane as well or only on the other

    layer?

    if yes, how do I route over the ground, as the routes need to cut space

    around them?

    tia.

    --

    "Dave" <dave@x.com> wrote in message

    news:0822l45msfhqis4vba9cnooefpmgd5p9t2@4ax.com...

    On Tue, 23 Dec 2008 15:19:59 -0000, <basicbrd@noreply.co.uk> wrote:

     

    >I am working on a 2 layer board. Should I be using a ground

    >plane, and if so how do I add it and perform auto routing?

     

    Use the POLYGON command to create a copper pour.  This can be almost

    any shape you can think of.  IOW, it doesn't need to be a rectangle.

    Then use the NAME command to name the polygon GND.

    Note: The default line width of 16 mil (0.016") usually works well.

    However, if you have gaps in the pour, say between pads, then decrease

    the line width.  If you make the line width too narrow, you will

    create a huge Gerber file.

     

    -Dave Pollum

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Groundplanes aka. copper pours work in all Eagle versions,

    one way to make one is to type 'polygon gnd' and draw the outer edges of

    the groundplane to be.

    Before drawing you may also select stuff like width, hatch or solid, via

    thermals on/off etc.

     

    You can put groundplanes where you see fit, around the entire board or

    just in selected areas.

    When you then click ratsnest the pour is drawn, and automatically avoids

    routed tracks,

    and 'isolate' sets the isolation distance between tracks and pour.

     

    Well, I have just tried what  you said and I can see you are right about

    this.

    Is this also explained in the eagle tutorial, or elsewhere?