Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle freezes if run from ulp to generate gerber files
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Subscribers 189 subscribers
  • Views 2442 views
  • Users 0 members are here
Related

Eagle freezes if run from ulp to generate gerber files

e14 Contributor
e14 Contributor over 12 years ago

I have a ULP to automate generation of gerberfiles.

In the ULP I use the following command:

 

system("\"" + EagleExe + "\" -X -x0.0 -y0.0 -O+ -c- -dGERBER_RS274X -o\"" + GerberFileName + "\" \"" + B.name + "\" tPlace tNames");

 

This usually works fine but in some cases it just freezes and nothing happens.

If I run the CAM processor manually i get the following warning:

Fullscreen contentimage_31710.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

The ULP probably freezes because of this warning, but the warning is not shown.

Eagle is probably waiting for me to answer the non visible dialog.

Is there some "silent mode" without warnings or some other way to sole this problem?

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 12 years ago

    Not sure why, but Eagle is waiting for input from the stdin.  Even if

    stdin is not a tty, it sits there and waits.

     

    I managed to fix this by echoing an "n" to stdin.  It's been working

    consistently ever since.  Even if it never eats the character, there's

    one ready to be read.  Here's a few lines I use to generate a complete

    set of gerber files:

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-TopCopper.gbr 516800.brd 1 17 18 || exit 1

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-BotCopper.gbr 516800.brd 16 17 18 || exit 1

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-NonPTHoles.gbr 516800.brd 20 || exit 1

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-TopSilkScreen.gbr 516800.brd 21 25 || exit 1

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-BotSilkScreen.gbr 516800.brd 22 26 || exit 1

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-TopMask.gbr 516800.brd 29 || exit 1

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-BotMask.gbr 516800.brd 30 || exit 1

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-TopPaste.gbr 516800.brd 31 || exit 1

     

    echo n | eagle -X -N- -f+ -O+ -c- -x0 -y0 -dGERBER_RS274X -o

    516800-RevA-BotPaste.gbr 516800.brd 32 || exit 1

     

    echo n | eagle -X -f+ -N- -O+ -c- -x0 -y0 -E+0.1 -R 516800-RevA.drl

    -dEXCELLON -o 516800-RevA-ExcellonDrill.exc 516800.brd 44 45 || exit 1

     

     

    HTH,

        - Chuck

     

     

     

    On 02/17/2014 06:02 AM, Magnus H-C wrote:

    I have a ULP to automate generation of gerberfiles.

    In the ULP I use the following command:

     

    system("\"" + EagleExe + "\" -X -x0.0 -y0.0 -O+ -c- -dGERBER_RS274X

    -o\"" + GerberFileName + "\" \"" + B.name + "\" tPlace tNames");

     

    This usually works fine but in some cases it just freezes and nothing

    happens.

    If I run the CAM processor manually i get the following warning:

     

    The ULP probably freezes because of this warning, but the warning is not

    shown.

    Eagle is probably waiting for me to answer the non visible dialog.

    Is there some "silent mode" without warnings or some other way to sole

    this problem?

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/104018

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dukepro

    Thank you!

    This works great, but since I use a ULP and (I think) you use a bat-file i had to add "CMD.EXE /c echo y | " in the system call.


    system("CMD.EXE /c echo y | \"" + EagleExe + "\" -X -x0.0 -y0.0 -O+ -c- -dGERBER_RS274X -o\"" + GerberFileName + "\" \"" + B.name + "\" Top Pads Vias");

     

    Simple explanation of variables used:

    "EagleExe" is a string set to the full path of Eagle.exe

    "GerberFileName" is a string set to output path and filename

    B.name is the filename of the board




     



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 12 years ago in reply to e14 Contributor

    On 02/18/2014 11:29 AM, Magnus H-C wrote:

    Thank you!

    This works great, but since I use a ULP and (I think) you use a bat-file

    i had to add "CMD.EXE /c echo y | " in the system call.

     

    Excellent.  Glad it worked out for you.

     

    The excerpt I posted earlier is part of a shell script that is created

    from a ULP, then just prior to exiting, the ULP calls

    system("./camprep.sh &"); where the ampersand causes the script to be

    executed in the background, thus causing the system() call to return

    immediately, which, in turn, allows Eagle to continue executing while

    the CAM jobs are being created.  I don't know if Windows has some

    equivalent, but you may consider having the argument to system() execute

    in the background - just to prevent freezes.

     

    The ULP determines from the board design which gerber/Excellon files

    need to be created, and which layers to include with each.  The script

    includes the recursive removal of a directory and recreation of it.

    Then all the output files and the associated .gpi files are moved to

    this new directory, and a zip file of the gerbers is created ready for

    uploading to the board fabricator.

     

    So, all in all, it's a clean way to generate a zipped collection of

    gerbers for a particular design - just "run camprep" in the Eagle

    command line.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dukepro

    Hey Chuck,

     

    great, thanks!

     

    Best regards,

    Lieven.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dukepro

    Hey Chuck,

     

    great, thanks!

     

    Best regards,

    Lieven.