EAGLE User Support (English) Designing A Circuit As A Complete Newbie
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 180 subscribers
  • Views 371 views
  • Users 0 members are here
  • fans
Related

Designing A Circuit As A Complete Newbie

Former Member
Former Member over 12 years ago

I'm building a robot in my class and we're required to design our own personalized circuit board for it, however I really don't understand anything about this, so if you could help me in the simplest terms that would be amazing. Basically, my robot is going to have to be hooked up to four separate computer fans that I can control independently. I guess I was just wondering how I start with this? -.- I'm so lost I don't even know how to ask a proper question...

 

I have a blank schematic and I just want to make a circuit that can run four fans. Can someone help me? I really have no idea what I'm doing.

  • Sign in to reply
  • Cancel
  • saurocksall
    0 saurocksall over 12 years ago

    Hi Johanna,

     

    Can you specify what task your robot needs to perform ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 22/02/2014 7:13 a.m., Dallis King wrote:

    I'm building a robot in my class and we're required to design our own

    personalized circuit board for it, however I really don't understand

    anything about this, so if you could help me in the simplest terms that

    would be amazing. Basically, my robot is going to have to be hooked up

    to four separate computer fans that I can control independently. I guess

    I was just wondering how I start with this? -.- I'm so lost I don't even

    know how to ask a proper question...

     

    I have a blank schematic and I just want to make a circuit that can run

    four fans. Can someone help me? I really have no idea what I'm doing.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/104471

     

     

     

    This forum is for the support of the use of EagleCad software and not

    for education on electronic design. You would be best to Google for the

    many sites that cater for robotics development if you are starting from

    nothing.

     

    That said, maybe you have been given the circuit you have to work with

    and the exercise is to create the circuit board from the schematic you

    have been provided with, you haven't said.

     

    Is the use of Eagle the required approach for the class. Talk to your

    class mates and tutor about the approaches they are taking.

     

    Whatever the case, you need to start into one of the many tutorials

    there are for Eagle or the alternate PCB CAD programs on the net.

    YouTube videos will give you an appreciation of how a program works

    most quickly, then after that you should read and perform the exercises

    in written tutorials as only then will you learn and remember how to use

    the chosen CAD program.

     

    All the best

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to autodeskguest

    You're kind of starting at the wrong end looking at a blank schematic.

    First, you need to do some research and information gathering.  You need to

    determine what it takes to control the fans (what circuit do you need).  Is

    the controller for the fans smart or just what kind of information does it

    need to process to figure out what to do with the fans - I would assume the

    4 fans are supposed to be controlled some how - what controls them? is

    there a remote control or? that determines what the fans do.  Once you have

    determined the requirements for the project, then you come up with a block

    diagram of how it all fits together.  Next come up with sketches of what

    the actual control for the fan needs to be (simple transistor driven by a

    little processor (PIC for example)) or just what?  Leaping into drawing a

    schematic before you have worked out the requirements is like writing code

    before you have figured out what you want to do.  Once you have that nailed

    down, then you can work on putting a schematic into Eagle or whatever, but

    first you need to come up with the requirements and do the details.  Yeah,

    I know, not as much fun as jumping into the schematic, but it really is the

    right way to go.

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.