EAGLE User Support (English) Connection 3+ components
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 247 views
  • Users 0 members are here
Related

Connection 3+ components

Former Member
Former Member over 11 years ago

Hello.

I have connection between 3+ components in 1 point. When I convert schematic to board Eagle decide there to make connections between those components by himself.

I mean components 1, 2, 3 connected to 1 junction in a schematic, on board component 1 connected with component 2, component 2 with component 3. And I want component 1 with component 2, component 1 with component 3. It is correct but I can't make auto routing.

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 22/02/2014 9:49 a.m., Zakhar Khadanovich wrote:

    Hello.

    I have connection between 3+ components in 1 point. When I convert

    schematic to board Eagle decide there to make connections between those

    components by himself.

    I mean components 1, 2, 3 connected to 1 junction in a schematic, on

    board component 1 connected with component 2, component 2 with component

    3. And I want component 1 with component 2, component 1 with component

    3. It is correct but I can't make auto routing.

     

     

    Hello

     

    Hold down CTL key to route from a trace that is already routed when

    there is no airwire. You could also route from each component to the

    star point(junction). You can also 'RATSNEST'  at any time to have the

    airwires re-calculated.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 11 years ago in reply to autodeskguest

    On 02/21/2014 08:52 PM, warrenbrayshaw wrote:

    On 22/02/2014 9:49 a.m., Zakhar Khadanovich wrote:

    Hello.

    I have connection between 3+ components in 1 point. When I convert

    schematic to board Eagle decide there to make connections between those

    components by himself.

    I mean components 1, 2, 3 connected to 1 junction in a schematic, on

    board component 1 connected with component 2, component 2 with component

    3. And I want component 1 with component 2, component 1 with component

    3. It is correct but I can't make auto routing.

     

    Hello

     

    Hold down CTL key to route from a trace that is already routed when

    there is no airwire. You could also route from each component to the

    star point(junction). You can also 'RATSNEST'  at any time to have the

    airwires re-calculated.

     

    HTH

    Warren

     

    The air wires are always the shortest distance between the two nets.  In

    your example, component 3 is closer to component 2 than it is to

    component 1.  Hence the air wire is from 2 to 3.

     

    If you want to somewhat mirror what you have on the schematic, route

    from 1 to the common point representing the junction, then to 2.  Then

    route from 3 to the common point.

     

    HTH,

        - Chuck