Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Can't Load Old Schematic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 189 subscribers
  • Views 2008 views
  • Users 0 members are here
  • message
  • error
Related

Can't Load Old Schematic

e14 Contributor
e14 Contributor over 12 years ago

I have a schematic I did 2 years ago and now want to edit, but when I try to load it I get this error message: line 16474, column 66: redefinition of name 'SUPPLY1' in tag <part>. How can I fix this (or bypass it)?

 

Thanks,

Greg

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    Warren, you're right!  And going to the specified coordinates I found that there was a component missing in the edited file.  So I'm hoping that just replacing/reconnecting this component will fix the problem completely.

     

    I hadn't tried setting the grid to mm because I didn't think it was that big, but it is:  B size is 11x17 inches, so the width in mm is about 430.

     

    Thanks,

    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to e14 Contributor

    On 1/03/2014 6:48 a.m., Greg Marshall wrote:

    Doug, I actually tried that right after I posted the question.  In the

    first attempt it just went to another error involving the same signal,

    so I deleted that line also.  The schematic now loads and looks correct,

    but I'm sure there are missing connections.  A better 'hack' at this

    might be to change the signal name on these 2 lines to some new, unique

    name.  I haven't tried that yet.

     

    The 2nd error message is: <instance part="SUPPLY1" gate="GND" x="332.74"

    y="172.72"/>.  Note that this has coordinates in it, which I presume

    would indicate where the particular connection to this signal occurs,

    but what coordinate system is it?  I can only set the grid to 'normal'

    units such as inches or millimeters.

     

     

     

    The coordinate system for sch file is millimeters

     

    You can verify this for your self. Set the sch grid to MM. next locate a

    part on the schematic, say R1 and view its INFORMATION. Record its xy

    location

     

    Now look for the part in the file in the 'instances> instance' section.

    It will be towards the bottom. It will have the same XY there.

     

    Quickest way to find the right line is search in the file for "x="60.96"

    inserting the x you noted from INFORMATION. THere will likely only be

    one fine result, the one you want.

     

    Setting the grid to inches, performing a save and then inspecting the

    file again, there will be no change to the xy location of the part

    proving it's mm.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to AnalogNotes

    Doug, I actually tried that right after I posted the question.  In the first attempt it just went to another error involving the same signal, so I deleted that line also.  The schematic now loads and looks correct, but I'm sure there are missing connections.  A better 'hack' at this might be to change the signal name on these 2 lines to some new, unique name.  I haven't tried that yet.

     

    The 2nd error message is: <instance part="SUPPLY1" gate="GND" x="332.74" y="172.72"/>.  Note that this has coordinates in it, which I presume would indicate where the particular connection to this signal occurs, but what coordinate system is it?  I can only set the grid to 'normal' units such as inches or millimeters.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • AnalogNotes
    0 AnalogNotes over 12 years ago

    Opening my mouth where I might not know what I'm talking about, but here goes anyway!  image

     

    If you open that file with a text editor, do you find "SUPPLY1" listed twice in that part?  It may be as easy as using your editor to change that name, or delete the extra definition line.

     

    Make a backup first...  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<