Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Doubts about autorouting and polygon filling
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 1830 views
  • Users 0 members are here
  • eagle
  • fill
  • netclass
  • polygon
  • autoroute
Related

Doubts about autorouting and polygon filling

rahul91rahul
rahul91rahul over 12 years ago

Hello.

 

Thank you for listening to my doubts.

 

I've two questions mainly related to routing in the board designs.

 

1. I usually design boards which have a lot of connections. Being a lazy person, and with the awesome autorouting capabilities of EAGLE, I prefer to autoroute everything. Now I've many connections which should have different widths, like the power lines should be thicker [20 to 25mils] while normal I/O wires can go down to 16 or even 12mils. What I do in that case is create different netclasses for different types of connections [set different widths, via diameters, and clearance values], and then autoroute it. It works absolutely perfectly.

Now in my current board design, I've a situation where I want the very same connection [net] to be 20mils at certain places and 12 mils at certain places. Using netclasses I can either set it to 20 or 12mils at a given time, not both. So I can only autoroute that connection at 20mils first, then remove [ripup] the part that should be 12mils and autoroute the same connection again [with 12mils netclass] to get the autoroute to route at 12mils.

So is there any other way I can solve this situation by routing the very same connection [net] at two or more different widths at different physical points on the board at the same time? That way I'll only have to autoroute the whole board just once. Any help will be appreciated. By the way, the autorouting capabilities of EAGLE are simply amazing. Thank you EAGLE team for that functionality.

 

 

2. Thank you again for taking the time to read my doubts. My second doubt regarding board designs is about the polygon filling [copper pouring] part. I usually design double-sided boards with both sides polygon fillings of Ground planes, and occasionally 5V or 3.3V fillings.It might be a stupid question but should I fill the layer before starting my routing, or do it after I've routed the board 100%?

Having already mentioned above that I usually use the autoroute capabilities of EAGLE, if I autoroute my boards after polygon filling, I get a message that "polygons may have fallen apart".

When I fill the board before routing, I need to make proper vias at different points so that both layer fillings are shorted at all points. And it also makes the routing part tougher for me or the autorouter [maybe I'm wrong].

On the other hand, the opposite is much easier, i.e. routing the board first and then doing the pouring.

I personally feel that the copper pouring should be done before the routing, because doing it after everything has been routed doesn't improve the connections according to me. Again, any advices on this topic will be greatly appreciated.

Thanks a lot for even taking the time to go over my doubts.

Any inputs will be greatly appreciated.

 

 

And thank you team EAGLE for this lovely piece of software. Without you all I would have given up PCB designing. You all make it easy.

Rahul Sharma.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 1/03/2014 7:51 a.m., Rahul Sharma wrote:

    Hello.

     

    Thank you for listening to my doubts.

     

    I've two questions mainly related to routing in the board designs.

     

    1. I usually design boards which have a lot of connections. Being a lazy

    person, and with the awesome autorouting capabilities of EAGLE, I prefer

    to autoroute everything. Now I've many connections which should have

    different widths, like the power lines should be thicker

    while normal I/O wires can go down to 16 or even 12mils. What I do in

    that case is create different netclasses for different types of

    connections ,

    and then autoroute it. It works absolutely perfectly.

    Now in my current board design, I've a situation where I want the very

    same connection to be 20mils at certain places and 12 mils at

    certain places. Using netclasses I can either set it to 20 or 12mils at

    a given time, not both. So I can only autoroute that connection at

    20mils first, then remove the part that should be 12mils and

    autoroute the same connection again to get the

    autoroute to route at 12mils.

    So is there any other way I can solve this situation by routing the very

    same connection at two or more different widths at different

    physical points on the board at the same time? That way I'll only have

    to autoroute the whole board just once. Any help will be appreciated. By

    the way, the autorouting capabilities of EAGLE are simply amazing. Thank

    you EAGLE team for that functionality.

     

     

    First, ensure you have read Chapter7 of the manual and chapter 15 of the

    tutorial. "Autorouter: A Brief Example".

    Both in the Docs folder of your installation. You probably have.

     

    To answer your question #1. No. Eagle cannot read your mind. You would

    have to give it some clues about which area needs what and there is no

    way to do that for a one pass solution.

     

    Your design will dictate the approach to take.

     

    The first is to Autoroute (AR) at the smallest width and then

    selectively widen the traces that you want wider. click click click.

    Just as Doug said.

     

    What you can do is to run the Autorouter (AR) twice. Place restrict

    rectangle/polygons on the tRestrict and bRestrict to keep it from

    routing in those areas. Perform one pass at the desired width for the

    signal then remove the restrict areas and run the AR again, with the

    settings for the other width . It will complete the routing using this

    new value.

     

    There is a disadvantage here that the portion that is routed actually

    becomes satisfied without considering the portion that is not so in some

    cases routing the remaining portion may be less efficient. So the method

    you spoke of will be better. It all depends on your design and the space

    available for the traces.

     

     

     

    2. Thank you again for taking the time to read my doubts. My second

    doubt regarding board designs is about the polygon filling [copper

    pouring] part. I usually design double-sided boards with both sides

    polygon fillings of Ground planes, and occasionally 5V or 3.3V

    fillings.It might be a stupid question but should I fill the layer

    before starting my routing, or do it after I've routed the board 100%?

    Having already mentioned above that I usually use the autoroute

    capabilities of EAGLE, if I autoroute my boards after polygon filling, I

    get a message that "polygons may have fallen apart".

    When I fill the board before routing, I need to make proper vias at

    different points so that both layer fillings are shorted at all points.

    And it also makes the routing part tougher for me or the autorouter

    .

    On the other hand, the opposite is much easier, i.e. routing the board

    first and then doing the pouring.

    I personally feel that the copper pouring should be done before the

    routing, because doing it after everything has been routed doesn't

    improve the connections according to me. Again, any advices on this

    topic will be greatly appreciated.

    Thanks a lot for even taking the time to go over my doubts.

    Any inputs will be greatly appreciated.

     

     

     

    Read AUTO in the HELP

    There it explains you can exclude a signal from the AR. So try this:

    Exclude the signals that can get a connection/interconnect via the

    polygon copper pour. AR the remainder and then do the ratsnest for the

    excluded signals (Likely ground, GND). If you are in luck all GND

    pads/SMD will be connected (non isolated). Check for remaining airwires.

    This is only good when you dont need to consider the ground loops in the

    copper pour as in mixed signal designs. You may have to preempt the

    result and drop a via in strategic places.

     

     

    From the above and what you read elsewhere, you will see why designers

    will manually route and if they use the AR it is used selectively.

     

    HTH

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rahul91rahul
    0 rahul91rahul over 12 years ago in reply to autodeskguest

    Thank you for your reply.

     

    I somewhat do it the way you explained. I selectively autoroute my connectoins. But I do the opposite of what you said. I first autoroute the thicker parts and then take care of the thinner parts. If I change the thinner to thicker I might get clearance issues.
    Even now I do the autorouting part twice for a connection like I mentioned in my question.

     

    For your reply to my 2nd question, I do the exact same thing - filling the board with GND pour first and then autorouting the remaining first. And then yes I'm too unlucky that I still get unrouted GND connections at some places. image But like you said again, I make certain vias and necessary connections again. I was just wondering if there's an easier and "lazier" approach to it. image

     

    So in the end, my board becomes a mix of manual and autoroutes. Not a problem though, but just wondered if there's one click setting for my requirement which I might have missed. I'm just a newbie afterall. And lazy. image

     

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rahul91rahul
    0 rahul91rahul over 12 years ago in reply to autodeskguest

    Thank you for your reply.

     

    I somewhat do it the way you explained. I selectively autoroute my connectoins. But I do the opposite of what you said. I first autoroute the thicker parts and then take care of the thinner parts. If I change the thinner to thicker I might get clearance issues.
    Even now I do the autorouting part twice for a connection like I mentioned in my question.

     

    For your reply to my 2nd question, I do the exact same thing - filling the board with GND pour first and then autorouting the remaining first. And then yes I'm too unlucky that I still get unrouted GND connections at some places. image But like you said again, I make certain vias and necessary connections again. I was just wondering if there's an easier and "lazier" approach to it. image

     

    So in the end, my board becomes a mix of manual and autoroutes. Not a problem though, but just wondered if there's one click setting for my requirement which I might have missed. I'm just a newbie afterall. And lazy. image

     

    Thank you.