Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Import scanned PCB artwork to create Eagle PCBs?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 2181 views
  • Users 0 members are here
  • board
  • artwork
  • schematic
  • magazine
  • scan
Related

Import scanned PCB artwork to create Eagle PCBs?

e14 Contributor
e14 Contributor over 12 years ago

I've successfully imported scanned PCB artwork layout from magazines into Eagle and would like to use that to create a circuit board.

Having imported the BMP into an empty board layout in Eagle I was hoping I could use that layer as a guide for placing the components as well as connecting them together but being a novice I'm not able to figure out how or if it's even possible.

It seems Eagle's way of doing things is to first create a schematic, then make a board out of that -not the other way round.

 

Is there a way I can use the scanned images in Eagle (I don't have/intend to buy any etching gear for the "photoresist" method or know anyone who can help me with that, so it seems easier to find a company which makes PCBs from Eagle generated files). I'm using Eagle 6.5.0 (Light edition) on a Mac.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    Mylist Address wrote:

     

    I've successfully imported scanned PCB artwork from magazines into Eagle

    and would like to use that to create a circuit board.

    Having imported the BMP into an empty board layout in Eagle I was hoping

    I could use that layer as a guide for placing the components as well as

    connecting them together but being a novice I'm not able to figure out

    how or if it's even possible.

    It seems Eagle's way of doing things is to first create a schematic,

    then make a board out of that -not the other way round.

     

    Is there a way I can use the scanned images in Eagle (I don't

    have/intend to buy any etching gear for the "photoresist" method or know

    anyone who can help me with that, so it seems easier to find a company

    which makes PCBs from Eagle generated files).

     

    have you thought about recreating the schematic in eagle too.

     

    The would get you 1) ERC and DRC capabilities and 2) the nets would be

    represented as air wires in the board editor automatically.

     

    You still can use your imported artwork as aid for placement and

    routing.

     

     

    On the other hand: you can do the layout without a schematic.

    You would add packages matching the required footprints, and using the

    signal command establish the connections (as air wires), then do the

    routing.

    But: you can't create a schematic from that layout.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago

    Mylist Address wrote:

     

    I've successfully imported scanned PCB artwork from magazines into Eagle

    and would like to use that to create a circuit board.

    Having imported the BMP into an empty board layout in Eagle I was hoping

    I could use that layer as a guide for placing the components as well as

    connecting them together but being a novice I'm not able to figure out

    how or if it's even possible.

    It seems Eagle's way of doing things is to first create a schematic,

    then make a board out of that -not the other way round.

     

    Is there a way I can use the scanned images in Eagle (I don't

    have/intend to buy any etching gear for the "photoresist" method or know

    anyone who can help me with that, so it seems easier to find a company

    which makes PCBs from Eagle generated files).

     

    have you thought about recreating the schematic in eagle too.

     

    The would get you 1) ERC and DRC capabilities and 2) the nets would be

    represented as air wires in the board editor automatically.

     

    You still can use your imported artwork as aid for placement and

    routing.

     

     

    On the other hand: you can do the layout without a schematic.

    You would add packages matching the required footprints, and using the

    signal command establish the connections (as air wires), then do the

    routing.

    But: you can't create a schematic from that layout.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    So you're saying that I can easily place the airwires in the exact same way as the scanned PCB artwork?

    How would I go about doing that?

    I've mainly used the autorouting feature.

     

    Yes, I agree that creating a schematic would be the best way if it's not too much additional work to place the wires/traces where they should be.