EAGLE User Support (English) QFN package and grid problems
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
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 364 views
  • Users 0 members are here
Related

QFN package and grid problems

Former Member
Former Member over 11 years ago

Hi All,

 

I am an Eagle 6.5.0 newbie image

 

I am trying to create a QFN pkg for a TI part.  Here are the details.

 

1) 4 pins on a side with 0.5mm pitch

2) pad size of 0.28x0.85 mm

 

The problem I am confronting is that all the dimensions are such that I need to constantly change grid resolution.  But for example when I create 4 of the pins on a side with 0.5mm grid and change the grid so I can create another side's 4 pins (2.1 mm away), I CANNOT measure that distance since the MARK command only works on grid lines and the pads are not aligned to any grids.

 

Question 1:  What is the proper way to do this when a whole bunch of dimensions are used and require different grid resolutions. 

Question 2:  Is there a way to create a pad that is round on one end ?

 

many thanks in advanced.

 

image

  • Sign in to reply
  • Cancel
Parents
  • AnalogNotes
    0 AnalogNotes over 11 years ago

    For this part, have you tried setting the grid to 0.01mm?

     

    I don't know about round pad, maybe someone else can help with that...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • AnalogNotes
    0 AnalogNotes over 11 years ago

    For this part, have you tried setting the grid to 0.01mm?

     

    I don't know about round pad, maybe someone else can help with that...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer