EAGLE User Support (English) QFN package and grid problems
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
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 365 views
  • Users 0 members are here
Related

QFN package and grid problems

Former Member
Former Member over 11 years ago

Hi All,

 

I am an Eagle 6.5.0 newbie image

 

I am trying to create a QFN pkg for a TI part.  Here are the details.

 

1) 4 pins on a side with 0.5mm pitch

2) pad size of 0.28x0.85 mm

 

The problem I am confronting is that all the dimensions are such that I need to constantly change grid resolution.  But for example when I create 4 of the pins on a side with 0.5mm grid and change the grid so I can create another side's 4 pins (2.1 mm away), I CANNOT measure that distance since the MARK command only works on grid lines and the pads are not aligned to any grids.

 

Question 1:  What is the proper way to do this when a whole bunch of dimensions are used and require different grid resolutions. 

Question 2:  Is there a way to create a pad that is round on one end ?

 

many thanks in advanced.

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

     

    "Sadry Tavana" <noreply-237344@element14.com> a écrit dans le message de news:

    912995212.121394741978168.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    Hi All,

     

    I am an Eagle 6.5.0 newbie image

     

    I am trying to create a QFN pkg for a TI part. Here are the details.

     

    1) 4 pins on a side with 0.5mm pitch

    2) pad size of 0.28x0.85 mm

     

    The problem I am confronting is that all the dimensions are such that I

    need to constantly change grid resolution. But for example when I

    create 4 of the pins on a side with 0.5mm grid and change the grid so I

    can create another side's 4 pins (2.1 mm away), I CANNOT measure that

    distance since the MARK command only works on grid lines and the pads

    are not aligned to any grids.

     

    Question 1: What is the proper way to do this when a whole bunch of

    dimensions are used and require different grid resolutions.

    Question 2: Is there a way to create a pad that is round on one end ?

     

    many thanks in advanced.

     

    1) You can enter the coords manually for each pad without change the grid.

     

    2) You are probably talking about a "finger pad"

    You can partially recover your rectangular smd pad with a polygon or a wire

    See: "Arbitrary Pad Shape" in the PAD section of the EAGLE Help

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Thanks to both for helpful replies.  This resolved my problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Thanks to both for helpful replies.  This resolved my problem.