EAGLE User Support (English) Can't resolve implicit power pin conflicts.
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
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 179 subscribers
  • Views 927 views
  • Users 0 members are here
  • eagle
  • layout
  • pcb_layout
  • Design
Related

Can't resolve implicit power pin conflicts.

billpenner
billpenner over 11 years ago

How do I resolve the problem with implicit power pins not being allowed to co exist. When different ICs  on the same project have differing power/GND names. ie. GND and V- etc.Eagle will allow only one name when connecting the signals.I have read many discussions with some indicating that it can be turned off. Can someone please help? I am sure it must be simple but I have not been able to solve.

Thanks.

Bill

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 11 years ago

    Hi Bill,

     

    I think EAGLE doesn't care what the pin is named, just cares what the net is named. So, usually I just connect the pins as desired, and make sure the ground net is labelled something appropriate (e.g. 0V), supply is labelled 3V3 or similar, etc. EAGLE won't care if I connect 3V3 to VDD pins or VCC, etc.

    As I understand, there is no way to give a net two names without a component in-between (e.g. a star ground point), which is really then two nets anyway. Sometimes I do want to give a different name for information purposes near a connector for example, but in that case I work around it by just making a text note on the schematic (e.g. something like "Vin" or "Supply_out" even if they are connected to the same net).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago

    Hi Bill,

     

    I think EAGLE doesn't care what the pin is named, just cares what the net is named. So, usually I just connect the pins as desired, and make sure the ground net is labelled something appropriate (e.g. 0V), supply is labelled 3V3 or similar, etc. EAGLE won't care if I connect 3V3 to VDD pins or VCC, etc.

    As I understand, there is no way to give a net two names without a component in-between (e.g. a star ground point), which is really then two nets anyway. Sometimes I do want to give a different name for information purposes near a connector for example, but in that case I work around it by just making a text note on the schematic (e.g. something like "Vin" or "Supply_out" even if they are connected to the same net).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to shabaz

    On 16/03/14 03:34, shabaz wrote:

    I think EAGLE doesn't care what the pin is named, just cares what the

    net is named. So, usually I just connect the pins as desired, and make

    sure the ground net is labelled something appropriate (e.g. 0V), supply

    is labelled 3V3 or similar, etc. EAGLE won't care if I connect 3V3 to

    VDD pins or VCC, etc.

     

    I don't think that's quite true. If the power pin is named "VDD" and you

    connect it to a net called "3V3" then you get a warning in the ERC, but

    the connections are made correctly as you intend.

     

    If a component has a (hidden) pin marked as direction "power" and named

    "VDD", and if you have a net named "VDD" (with a supply symbol on it),

    and you leave that power pin uninvoked, then Eagle will automatically

    connect it to the net. This behaviour is convenient if all your

    components have the same power supply naming convention, but can be

    overridden with explicit connections if not.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer