EAGLE User Support (English) How to upgrade from EagleCad 6.4 to 6.5 without loosing the license?
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
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 312 views
  • Users 0 members are here
  • eagle
  • license
  • upgrade
Related

How to upgrade from EagleCad 6.4 to 6.5 without loosing the license?

lvignals
lvignals over 11 years ago

When a license is installed for EagleCad version 6.4, what is the procedure to upgrade from 6.4 EagleCad to version 6.5?

Do I need to backup the license file first?

Can I install both versions side by side?

Will the upgrade replace the existing version in place and pick-up the license that was already installed?

Does CadSoft/Element-14 documents the proper upgrade process in detail somewhere?

 

Thanks :-)

  • Sign in to reply
  • Cancel
  • dukepro
    0 dukepro over 11 years ago

    On 03/18/2014 06:03 PM, Lu Vi wrote:

    When a license is installed for EagleCad version 6.4, what is the

    procedure to upgrade from 6.4 EagleCad to version 6.5?

     

    You can install 6.5 beside 6.4.  Use the same license file and the same

    activation code.

     

    Will the upgrade replace the existing version in place and pick-up the

    license that was already installed?

     

    The default installation location on Linux is /opt/eagle-6.5.0.  This

    does not overwrite 6.4.  Installation will not automatically pickup the

    license.  Since you install Eagle as root, you can license it at the end

    of the installation process.  I don't know about Mac or Windows.

     

    HTH,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer