EAGLE User Support (English) Is it possible to create a custom library from all the parts you use in a design?
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
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 181 subscribers
  • Views 568 views
  • Users 0 members are here
Related

Is it possible to create a custom library from all the parts you use in a design?

Former Member
Former Member over 12 years ago

I have been using different parts from different libraries and now want to bring all of them into a single library. 

 

1) Is it possible to do this automatically so I do not have to copy every single part?

2) Is it possible to automatically point all the components in the schematic actually draw from the new custom library?

 

thanks very much!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    ezrcer wrote:

     

    I have been using different parts from different libraries and now want

    to bring all of them into a single library. 

     

    1) Is it possible to do this automatically so I do not have to copy

    every single part?

    2) Is it possible to automatically point all the components in the

    schematic actually draw from the new custom library?

     

    there was a tread a short time back about this topisc.

     

    In short, you use the exp-project-lbr.ulp (perhaps in the version that

    allows to restrict the export to the used packages, see the cadsoft

    download area for that) to create one library pre original library.

     

    you will need to rename the created libraries.

     

    then use the update command.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to autodeskguest

    Thanks.  I downloaded the ULP and ran it. 

     

    1) It created 2 .scr files in my project directory and also a new custom library which has all the parts as expected except that it brought all the resistors and packages from a library that I originally used.  Why didn't it only give me the 0603 one that I exclusively used in the design

     

    2) Should I run the .scr files and why were they generated?  I noticed if I exit and enter the design again, the .scr files disappear.

     

    3) Fianlly, it did NOT update the library name in my schematic parts.  It still points to the old libraries???  I even did a use the new library and clicked update all without success.  Still points to the old library.

     

    What am I doing wrong?

     

    thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to Former Member

    Just noticed this comment from above and I did not do this before using new library.  Is this required?

     

    " First stop using all libraries with "use -*

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago in reply to Former Member

    Just noticed this comment from above and I did not do this before using new library.  Is this required?

     

    " First stop using all libraries with "use -*

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 12 years ago in reply to Former Member

    OK, I think I figured it out.  You need to run update with the following parameters to actually populate the new library parts into the schematics.

     

    UPDATE old_library_name = new_library_name;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer