EAGLE User Support (English) Eagle 6.5.0 for OSX 10.9.1 file open dialog boxes always open to "Documents" folder by default. Help?
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 377 views
  • Users 0 members are here
Related

Eagle 6.5.0 for OSX 10.9.1 file open dialog boxes always open to "Documents" folder by default. Help?

Former Member
Former Member over 11 years ago

This is a pretty minor problem, but it's been bugging me for ages.

 

When I first installed Eagle, selecting File>Open>Schematic would open a dialog box with my ~/ Documents/eagle folder opened by default. Likewise, editing or using library files would default to my library folder.

 

For some reason, now every dialog box that opens opens to the /Documents folder.  This is majorly annoying as I have to navigate to the /Applications/Eagle-6.5.0/lib folder any time I want to add a library to a project.

 

Here's what I've tried so far to resolve the problem:

 

I checked my Options>Directories and verified that they were all set right. Originally $EAGLEDIR somehow got set to nothing, so I updated my .bash_profile to point it to my install directory.  This still didn't fix the problem.

 

I tried uninstalling (deleting the program file) and installing a fresh copy of Eagle from a download, but it didn't fix the problem.

 

I uninstalled again and deleted the OSX install receipt, but still no change.

 

I know this problem seems minor, but it's super frustrating because I remember that it used to work!  Please help!

 

Thanks.

  • Sign in to reply
  • Cancel
  • rossw
    0 rossw over 11 years ago

    I was just about to start a new thread on this very topic - luckily I saw Michael's post first.

     

    I have Eagle 6.5.0 installed on my Windows laptop and MacBook and the problem only happens with the Mac version. What's frustrating to me is I have custom ULPs which I then have to locate manually every time I want to run them.