EAGLE User Support (English) Eagle CAD, custom part connect it to Plane
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
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 414 views
  • Users 0 members are here
Related

Eagle CAD, custom part connect it to Plane

Former Member
Former Member over 11 years ago

Hello,

 

I created a custom SMD part (a negative battery contact pad) the pad is part of the GND Net in the schematic... To my suprise, when I created the GND Plane, this pad is completely isolated from the plane (plane is Named GND) and was expecting the contact pad to have a thermal-type connection to the plane... however, it is isolated instead.

 

Did I forget something when creating the part, or forget something somehwere else?

 

How do I get this pad connected to it's associated plane?

 

Thank you!

-chuck

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 27/03/2014 6:02 a.m., Chuck Van Dien wrote:

    Hello,

     

    I created a custom SMD part (a negative battery contact pad) the pad is

    part of the GND Net in the schematic... To my suprise, when I created

    the GND Plane, this pad is completely isolated from the plane (plane is

    Named GND) and was expecting the contact pad to have a thermal-type

    connection to the plane... however, it is isolated instead.

     

    Did I forget something when creating the part, or forget something

    somehwere else?

     

    How do I get this pad connected to it's associated plane?

     

     

    In the schematic, it is likely the net is not connected to the battery

    negative pin. Move the battery and confirm the attached nets move also.

     

    You may also check that ensure the name of the net connected to the

    battery negative is named GND.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Thanks Warren, when I re-checked the schematic, I found a typo when I named the Plane! So, you were correct. Thank you.

     

    New problem... is there a way to make the thermal connection to the pad larger ***without*** increasing the width of the outline of the plane/polygon?

     

    Thank you!

    -c

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    Chuck Van Dien wrote:

     

    Thanks Warren, when I re-checked the schematic, I found a typo when I

    named the Plane! So, you were correct. Thank you.

     

    New problem... is there a way to make the thermal connection to the pad

    larger **without** increasing the width of the outline of the

    plane/polygon?

     

    yes and no ...

     

    you could switch off the thermals completely for that polygon

     

    or draw a small polygon (same net, wider outline) just around the pin

     

    or just draw trace stubs starting from the pin

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Thank you. Helpful anser!

    -c