EAGLE User Support (English) Edit NET list directly?
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 180 subscribers
  • Views 768 views
  • Users 0 members are here
Related

Edit NET list directly?

Former Member
Former Member over 11 years ago

Hello,

 

In order to get my via connected to Planes, I had to rename them... however, I mistakenly named 2 vias the *wrong* plane name... and when I attempt to re-rename it to correct it, it renames the entire NET !!! When I attempt to delete the via, it is directing me to the schematic, and there are no vias on the schematic...

 

I deleted the Plane, but the 2 vias are still linked to the wrong NET...

 

 

Simplist way should be to edit the NET directly, but I don't see anyway to invoke a NET Editor if one exists...

 

I would prefer *not* to use a backup which is several hours old and loose all this work since the last backup.

 

Suggestions?

 

Thank you!

-chuck

  • Sign in to reply
  • Cancel
  • AnalogNotes
    0 AnalogNotes over 11 years ago

    If you are using EAGLE 6, you can use a text editor to edit the board file directly...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • AnalogNotes
    0 AnalogNotes over 11 years ago

    Another thought...you might be able to use the ripup command to remove the via...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Chuck Van Dien wrote on Thu, 27 March 2014 07:46

    Hello,

     

    In order to get my via connected to Planes, I had to rename them...

    however, I mistakenly named 2 vias the wrong plane name... and when

    I

    attempt to re-rename it to correct it, it renames the entire NET !!!

    When I attempt to delete the via, it is directing me to the schematic,

    and there are no vias on the schematic...

     

    I deleted the Plane, but the 2 vias are still linked to the wrong

    NET...

     

     

    Simplist way should be to edit the NET directly, but I don't see

    anyway

    to invoke a NET Editor if one exists...

     

    I would prefer not to use a backup which is several hours old and

    loose all this work since the last backup.

     

    Suggestions?

     

     

    Use RIPUP on the vias.

     

    The backups that eagle makes should not be hours old. It will backup every

    few minutes depending on the settings you have auto backup configured for

    and more often each time you save the editor.

     

    HTH

    Warren

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.