EAGLE User Support (English) Connect two different NETs
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
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 182 subscribers
  • Views 1957 views
  • Users 0 members are here
  • eagle
  • connect
  • netlist
  • nets
Related

Connect two different NETs

MaxKielland
MaxKielland over 11 years ago

This isn't that simple as it first sounds. Assume the following scenario.

Fullscreen contentimage_30700.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

The red signal, LOAD+ is dimensioned for 10A but the green signal, Feed back, is going to an OP-AMP and only needs a few mA. Is there any way I can connect these two nets without automatically rename one of them?

 

Do I really have to put in a 0 resistor because of limitations in EAGLE?

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 11 years ago

    On 03/26/2014 04:25 PM, Max Kielland wrote:

    This isn't that simple as it first sounds. Assume the following

    scenario.

    The red signal, LOAD+ is dimensioned for 10A but the green signal, Feed

    back, is going to an OP-AMP and only needs a few mA. Is there any way I

    can connect these two nets without automatically rename one of them?

     

    Max,

     

    As Rob mentioned, the best way to short two nets together is with a

    package that has two SMD's that overlap.  DRC will complain about the

    overlap, but since it is intentional, it can be safely approved.

     

    Attached is an abbreviated library providing an example of a short.

    Using the provided package as an example, you can create shorts with

    preferred widths and add them to the device.

     

    HTH,

        - Chuck

     

     

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 11 years ago

    On 03/26/2014 04:25 PM, Max Kielland wrote:

    This isn't that simple as it first sounds. Assume the following

    scenario.

    The red signal, LOAD+ is dimensioned for 10A but the green signal, Feed

    back, is going to an OP-AMP and only needs a few mA. Is there any way I

    can connect these two nets without automatically rename one of them?

     

    Max,

     

    As Rob mentioned, the best way to short two nets together is with a

    package that has two SMD's that overlap.  DRC will complain about the

    overlap, but since it is intentional, it can be safely approved.

     

    Attached is an abbreviated library providing an example of a short.

    Using the provided package as an example, you can create shorts with

    preferred widths and add them to the device.

     

    HTH,

        - Chuck

     

     

     

    Attachments: