EAGLE User Support (English) Connect two different NETs
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
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 182 subscribers
  • Views 1963 views
  • Users 0 members are here
  • eagle
  • connect
  • netlist
  • nets
Related

Connect two different NETs

MaxKielland
MaxKielland over 11 years ago

This isn't that simple as it first sounds. Assume the following scenario.

Fullscreen contentimage_30700.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

The red signal, LOAD+ is dimensioned for 10A but the green signal, Feed back, is going to an OP-AMP and only needs a few mA. Is there any way I can connect these two nets without automatically rename one of them?

 

Do I really have to put in a 0 resistor because of limitations in EAGLE?

  • Sign in to reply
  • Cancel
Parents
  • MaxKielland
    0 MaxKielland over 11 years ago

    Now when I read my own question a few days later I realize that I have been give too litle information. It isn't the Schematic that is the real "problem", it is the PCB routing. Since LOAD+ is dimensioned for 10A and the sense (feedback) only draws a few mA, I dont want (or can because of OP pin spacing) have it dimensioned for 10A.

     

    Making an overlapping land pad might be one solution to get "around" this problem. But if I have to accept the overlapping, I could just accept the feedback trace to be smaller than the 10A trace.

     

    Thanks to everyone contributing....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • AnalogNotes
    0 AnalogNotes over 11 years ago in reply to MaxKielland

    Are you using the autorouter?  I've only routed manually, so I always choose an appropriate trace width myself...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • AnalogNotes
    0 AnalogNotes over 11 years ago in reply to MaxKielland

    Are you using the autorouter?  I've only routed manually, so I always choose an appropriate trace width myself...