EAGLE User Support (English) Connecting TRACE to VIA?
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
  • State Not Answered
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 2684 views
  • Users 0 members are here
Related

Connecting TRACE to VIA?

Former Member
Former Member over 11 years ago

Hello,

 

1st-time Eagle 6.5 user here...

 

In order to get my vias to connect to their respective ground or poser plane, I had to rename them to the plane name...

 

Question: Are vias automatically connected to Trace/Routes? Or do they also need to be renamed, and if so, what name do I use? The Route name or the NET name?

 

The rubber-banding does not connect to them - so assuming they are *not* connected. Don't want to add vias to the schematic... so, assuming they have to be added toi the NET, but don't know the proper procedure.

 

Thank you for your help.

-chuck

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 27/03/14 16:16, Chuck Van Dien wrote:

    The rubber-banding does not connect to them - so assuming they are not

    connected. Don't want to add vias to the schematic... so, assuming they

    have to be added toi the NET, but don't know the proper procedure.

     

    You probably aren't making this mistake, but just in case...

     

    Some people make the mistake of thinking they have to place vias, name

    them to match the nets, then route through them. That's not the way to

    work. When you are routing a net, starting on the top layer, then you

    find you need to change to the bottom, just click the middle mouse

    button. The next bit of trace will then be placed on the other side, and

    as soon as you click to drop a corner the necessary via is added

    automatically.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 27/03/14 16:16, Chuck Van Dien wrote:

    The rubber-banding does not connect to them - so assuming they are not

    connected. Don't want to add vias to the schematic... so, assuming they

    have to be added toi the NET, but don't know the proper procedure.

     

    You probably aren't making this mistake, but just in case...

     

    Some people make the mistake of thinking they have to place vias, name

    them to match the nets, then route through them. That's not the way to

    work. When you are routing a net, starting on the top layer, then you

    find you need to change to the bottom, just click the middle mouse

    button. The next bit of trace will then be placed on the other side, and

    as soon as you click to drop a corner the necessary via is added

    automatically.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.