EAGLE User Support (English) Connecting TRACE to VIA?
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
  • State Not Answered
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 2669 views
  • Users 0 members are here
Related

Connecting TRACE to VIA?

Former Member
Former Member over 11 years ago

Hello,

 

1st-time Eagle 6.5 user here...

 

In order to get my vias to connect to their respective ground or poser plane, I had to rename them to the plane name...

 

Question: Are vias automatically connected to Trace/Routes? Or do they also need to be renamed, and if so, what name do I use? The Route name or the NET name?

 

The rubber-banding does not connect to them - so assuming they are *not* connected. Don't want to add vias to the schematic... so, assuming they have to be added toi the NET, but don't know the proper procedure.

 

Thank you for your help.

-chuck

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    The vias that I add after-ther fact, have been to tie ground or power planes together.

     

    But, when routing this is good to know, I have been routing on one side and then changing the property on the "leg" to the other side... but, good to know about the middle mouse button... being a 2 mouse button guy (on the MAC running VMWare) is there a key/mouse button combination for 2 button mouse users who want to use this feature? I tried, "Help Mouse" but there was no help available for "mouse".

     

    Thank you for the detailed reply, it is very helpful.

     

    -chuck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    The vias that I add after-ther fact, have been to tie ground or power planes together.

     

    But, when routing this is good to know, I have been routing on one side and then changing the property on the "leg" to the other side... but, good to know about the middle mouse button... being a 2 mouse button guy (on the MAC running VMWare) is there a key/mouse button combination for 2 button mouse users who want to use this feature? I tried, "Help Mouse" but there was no help available for "mouse".

     

    Thank you for the detailed reply, it is very helpful.

     

    -chuck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    Chuck Van Dien wrote:

    The vias that I add after-ther fact, have been to tie ground or power

    planes together.

     

    in that case I'd suggest you type "via 'netname' " on the

    command line and then click wherever you want to place a via of that

    net.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 28/03/2014 11:21 a.m., Chuck Van Dien wrote:

    The vias that I add after-ther fact, have been to tie ground or power

    planes together.

     

    But, when routing this is good to know, I have been routing on one side

    and then changing the property on the "leg" to the other side... but,

    good to know about the middle mouse button... being a 2 mouse button guy

    (on the MAC running VMWare) is there a key/mouse button combination for

    2 button mouse users who want to use this feature? I tried, "Help Mouse"

    but there was no help available for "mouse".

     

    HI Chuck

    What you could do , assuming you are only interested in changing between

    the top and bottom layers, is to assign a couple of keys.

     

    On a windows keyboard it is comfortable to assign Alt + A and ALT + S

    In that way the mouse hand can stay on the mouse and the left hand can

    do the swapping between layers.

     

    So enter into the command line

    ASSIGN A+A layer 1

    ASSIGN A+S layer 16

     

    HTH

    Warren
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.